<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: ADC readings on FRDM KL25Z in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-readings-on-FRDM-KL25Z/m-p/388266#M21013</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;P&gt;Hi, P/N for part number, which op amp is recommended to interface the ADC? &lt;/P&gt;&lt;P&gt;I tried the example code in the help page, it still doesn't work, most probably the impedance seen at the 3.3v pin is high/very high.&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 12 Nov 2014 10:10:07 GMT</pubDate>
    <dc:creator>Matt85</dc:creator>
    <dc:date>2014-11-12T10:10:07Z</dc:date>
    <item>
      <title>ADC readings on FRDM KL25Z</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-readings-on-FRDM-KL25Z/m-p/388262#M21009</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I configured the ADC for the FRDM KL25Z board as in:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/45893i2F53F2B5821C95D9/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;This is my code:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; (void)AD1_Calibrate(TRUE);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; for(;;) {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; (void)AD1_Measure(TRUE); /* do conversion and wait for the result */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; (void)AD1_GetValue16(&amp;amp;value); /* get the result into value variable */&lt;/P&gt;&lt;P&gt;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The readings are (with the PTD5 pin connected to 3.3v):&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/46083i75F23E2D5FD27DD6/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;IMG alt="" class="jiveImage" style="max-width: 1200px; max-height: 900px;" /&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;any idea?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 08 Nov 2014 16:38:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-readings-on-FRDM-KL25Z/m-p/388262#M21009</guid>
      <dc:creator>Matt85</dc:creator>
      <dc:date>2014-11-08T16:38:05Z</dc:date>
    </item>
    <item>
      <title>Re: ADC readings on FRDM KL25Z</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-readings-on-FRDM-KL25Z/m-p/388263#M21010</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Matt,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) From&amp;nbsp; the waveform , it seems that it haven't input signal in ADC0_SE6b pin, I suggest you check the pin&amp;nbsp; use&amp;nbsp; scope;&lt;/P&gt;&lt;P&gt;2) I suggest that before read the result , measure the complete status ,&amp;nbsp; the detail code you can refer to the "help on component ";&lt;/P&gt;&lt;P&gt;3) You can change anther pin to try .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Nov 2014 02:28:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-readings-on-FRDM-KL25Z/m-p/388263#M21010</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2014-11-10T02:28:00Z</dc:date>
    </item>
    <item>
      <title>Re: ADC readings on FRDM KL25Z</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-readings-on-FRDM-KL25Z/m-p/388264#M21011</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;P&gt;Hi, thanks for your reply, I will try your suggestions. &lt;/P&gt;&lt;P&gt;Do you know if I need a buffer (voltage follower) at the adc input? Is it mandatory? In case it is, which P/N is suggested? Thanks&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Nov 2014 15:29:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-readings-on-FRDM-KL25Z/m-p/388264#M21011</guid>
      <dc:creator>Matt85</dc:creator>
      <dc:date>2014-11-10T15:29:43Z</dc:date>
    </item>
    <item>
      <title>Re: ADC readings on FRDM KL25Z</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-readings-on-FRDM-KL25Z/m-p/388265#M21012</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Matt,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Use the convenience pin , i test use the ADC0_SE0;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think whether need&amp;nbsp; voltage follower is rely on your input analog signal , is is a stable direct current signal , it needn't voltage follower .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Nov 2014 03:25:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-readings-on-FRDM-KL25Z/m-p/388265#M21012</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2014-11-11T03:25:32Z</dc:date>
    </item>
    <item>
      <title>Re: ADC readings on FRDM KL25Z</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-readings-on-FRDM-KL25Z/m-p/388266#M21013</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;P&gt;Hi, P/N for part number, which op amp is recommended to interface the ADC? &lt;/P&gt;&lt;P&gt;I tried the example code in the help page, it still doesn't work, most probably the impedance seen at the 3.3v pin is high/very high.&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Nov 2014 10:10:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-readings-on-FRDM-KL25Z/m-p/388266#M21013</guid>
      <dc:creator>Matt85</dc:creator>
      <dc:date>2014-11-12T10:10:07Z</dc:date>
    </item>
  </channel>
</rss>