<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Error J-Link in Kwikstik</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Error-J-Link-in-Kwikstik/m-p/188574#M2097</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;I'm using the KwikStick Demo Board (Kinetis k40-Freescale) to evaluation of a project with the CodeWarrior.&lt;/P&gt;&lt;P&gt;I do the connection by J-Link.&lt;/P&gt;&lt;P&gt;The board was functioning normally, but suddenly appear an error and I can no longer connect to it.&lt;/P&gt;&lt;P&gt;The error that appears when I'll debug is the following:&lt;/P&gt;&lt;P&gt;&lt;FONT color="#FF0000"&gt;“Launching Kwikstik_Demo_Kwikstikk40x256_Int_Flash_Debug_Segger J-Link” has encountered&amp;nbsp; a problem.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#FF0000"&gt;Failed to resume target process., Reset has failed.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;What may be happening with my board? Someone could help me?&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Rafael&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 08 Dec 2011 01:41:17 GMT</pubDate>
    <dc:creator>rafaelwerneck0</dc:creator>
    <dc:date>2011-12-08T01:41:17Z</dc:date>
    <item>
      <title>Error J-Link in Kwikstik</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Error-J-Link-in-Kwikstik/m-p/188574#M2097</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;I'm using the KwikStick Demo Board (Kinetis k40-Freescale) to evaluation of a project with the CodeWarrior.&lt;/P&gt;&lt;P&gt;I do the connection by J-Link.&lt;/P&gt;&lt;P&gt;The board was functioning normally, but suddenly appear an error and I can no longer connect to it.&lt;/P&gt;&lt;P&gt;The error that appears when I'll debug is the following:&lt;/P&gt;&lt;P&gt;&lt;FONT color="#FF0000"&gt;“Launching Kwikstik_Demo_Kwikstikk40x256_Int_Flash_Debug_Segger J-Link” has encountered&amp;nbsp; a problem.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#FF0000"&gt;Failed to resume target process., Reset has failed.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;What may be happening with my board? Someone could help me?&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Rafael&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Dec 2011 01:41:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Error-J-Link-in-Kwikstik/m-p/188574#M2097</guid>
      <dc:creator>rafaelwerneck0</dc:creator>
      <dc:date>2011-12-08T01:41:17Z</dc:date>
    </item>
    <item>
      <title>Re: Error J-Link in Kwikstik</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Error-J-Link-in-Kwikstik/m-p/188575#M2098</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Did you solve this problem? I have the same situation on my kwikstik after I was uploaded to flash program that used default processor expert configuration. I figured, probably this config by default lock device. That's strange because CW didn't displayed any warning or notice to prevent locking device. I've dried Jlink&amp;gt; unlock Kinetis but without success.&lt;/P&gt;&lt;P&gt;I can connect K40 via JLINK @ 4kHz or SWD @ 200kHz but I can't write/read/erase. Anyone have any idea to solve this problem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Apr 2012 03:37:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Error-J-Link-in-Kwikstik/m-p/188575#M2098</guid>
      <dc:creator>blankfield</dc:creator>
      <dc:date>2012-04-20T03:37:54Z</dc:date>
    </item>
  </channel>
</rss>