<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: MCU stress test?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCU-stress-test/m-p/385554#M20730</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Since I'm running the BSP_DEFAULT_IO_CHANNEL in polled mode the processor is always busy polling the UART so I was actually giving the processor a break by having it use dedicated hardware to perform math.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 16 Mar 2015 16:58:35 GMT</pubDate>
    <dc:creator>williamely</dc:creator>
    <dc:date>2015-03-16T16:58:35Z</dc:date>
    <item>
      <title>MCU stress test?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCU-stress-test/m-p/385553#M20729</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have been tasked with writing a function that causes the K64 to consume as much current as possible (not including GPIO) so I made a task that does a lot of floating point math on numbers generated by the RNGA and uses the MMCAU to encrypt the result.&lt;/P&gt;&lt;P&gt;I figured using more on-chip components (FPU, MMCAU, CRC, RNGA) would cause the current consumption and package temperature to increase but when I run the task current drops by about 1 mA.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone have a function that they use for this purpose?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Mar 2015 23:31:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCU-stress-test/m-p/385553#M20729</guid>
      <dc:creator>williamely</dc:creator>
      <dc:date>2015-03-13T23:31:07Z</dc:date>
    </item>
    <item>
      <title>Re: MCU stress test?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCU-stress-test/m-p/385554#M20730</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Since I'm running the BSP_DEFAULT_IO_CHANNEL in polled mode the processor is always busy polling the UART so I was actually giving the processor a break by having it use dedicated hardware to perform math.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Mar 2015 16:58:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCU-stress-test/m-p/385554#M20730</guid>
      <dc:creator>williamely</dc:creator>
      <dc:date>2015-03-16T16:58:35Z</dc:date>
    </item>
  </channel>
</rss>