<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: How to program K70 flash via USB ?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-program-K70-flash-via-USB/m-p/384844#M20667</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Sebastien:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What do you mean with this?:&lt;/P&gt;&lt;PRE _modifiedtitle="true" class="jive_text_macro jive_macro_quote"&gt;

&lt;P&gt;But now the extern part of the product is ready, this programation method needs the product to be took to pieces...&lt;/P&gt;
&lt;P&gt;&lt;/P&gt;
&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you mean that you cannot have a JTAG header connector in your custom board?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regarding your questions and some comments:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-&amp;nbsp;&amp;nbsp;&amp;nbsp; Bootloader is the most common solution. You can also try with EzPort interface; this is a serial (SPI) interface for an external device to program the flash memory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-&amp;nbsp;&amp;nbsp;&amp;nbsp; AN2295 is a serial bootloader (UART interface). It is not a USB solution.&lt;/P&gt;&lt;P&gt;-&amp;nbsp;&amp;nbsp;&amp;nbsp; You can use &lt;STRONG&gt;AN2295_TWR_K70120_cfg.h&lt;/STRONG&gt; or you can create your own file, e.g. &lt;STRONG&gt;My_K70_Board_cfg.h&lt;/STRONG&gt;. Just make sure the file matches your board schematic (UART channel, UART pins and GPIO pin if needed).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-&amp;nbsp;&amp;nbsp;&amp;nbsp; You are correct that &lt;STRONG&gt;FSL_Kinetis_Bootloader&lt;/STRONG&gt; only supports K64 right now, and it is focused in new Kinetis devices, so K70 has to wait.&lt;/P&gt;&lt;P&gt;-&amp;nbsp;&amp;nbsp;&amp;nbsp; There are some other application notes about Kinetis bootloaders. You may want to give them a check: &lt;STRONG&gt;AN4367&lt;/STRONG&gt;, &lt;STRONG&gt;AN4368&lt;/STRONG&gt;, &lt;STRONG&gt;AN4370&lt;/STRONG&gt;, &lt;STRONG&gt;AN4379&lt;/STRONG&gt;, &lt;STRONG&gt;AN4764&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; &lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 27 Aug 2014 21:25:39 GMT</pubDate>
    <dc:creator>Jorge_Gonzalez</dc:creator>
    <dc:date>2014-08-27T21:25:39Z</dc:date>
    <item>
      <title>How to program K70 flash via USB ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-program-K70-flash-via-USB/m-p/384843#M20666</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am running CodeWarrior for MCU 10.6 on Windows with a target of MK70FN1M0VMJ12. I don't use Freescale platform or board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Untill now I was programming with the PE micro Multilink Universal.&lt;/P&gt;&lt;P&gt;But now the extern part of the product is ready, this programation method needs the product to be took to pieces...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, I'd like to find a way to program the K70 flash via USB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That's why I read discussions, application notes (AN2295), and docs about the Kinetis Bootloader (KFLLDRUG, KBTLDRUG) but I couldn't find a clear solution...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a few questions, if anyone can help:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Is Bootloader a good option to resolve my problem ?&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;If yes:&lt;UL&gt;&lt;LI&gt;In the "AN2295SW.zip" (last version on freescale) , can I use "AN2295_TWR_K70120_cfg.h" even if I d'ont use the tower system ?&lt;/LI&gt;&lt;LI&gt;In the "AN2295SW.zip" (last version on freescale), there is no CW 10.6 folder and sources, is it a problem ?&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;UL&gt;&lt;UL&gt;&lt;LI&gt;Is the "FSL_Kinetis_Bootloader_1_0_2.zip" (last version on freescale), download via the Kinetis Bootloader page (&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KBOOT&amp;amp;fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1" title="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KBOOT&amp;amp;fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1"&gt;Kinetis Bootloader|Freescale&lt;/A&gt;) is only developped for the K64 ?&lt;/LI&gt;&lt;LI&gt;If yes, is a Kinetis Bootloader workink with K70 exists ?&lt;/LI&gt;&lt;/UL&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sébastien&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Aug 2014 16:00:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-program-K70-flash-via-USB/m-p/384843#M20666</guid>
      <dc:creator>sebastienpeyrau</dc:creator>
      <dc:date>2014-08-27T16:00:31Z</dc:date>
    </item>
    <item>
      <title>Re: How to program K70 flash via USB ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-program-K70-flash-via-USB/m-p/384844#M20667</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Sebastien:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What do you mean with this?:&lt;/P&gt;&lt;PRE _modifiedtitle="true" class="jive_text_macro jive_macro_quote"&gt;

&lt;P&gt;But now the extern part of the product is ready, this programation method needs the product to be took to pieces...&lt;/P&gt;
&lt;P&gt;&lt;/P&gt;
&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you mean that you cannot have a JTAG header connector in your custom board?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regarding your questions and some comments:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-&amp;nbsp;&amp;nbsp;&amp;nbsp; Bootloader is the most common solution. You can also try with EzPort interface; this is a serial (SPI) interface for an external device to program the flash memory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-&amp;nbsp;&amp;nbsp;&amp;nbsp; AN2295 is a serial bootloader (UART interface). It is not a USB solution.&lt;/P&gt;&lt;P&gt;-&amp;nbsp;&amp;nbsp;&amp;nbsp; You can use &lt;STRONG&gt;AN2295_TWR_K70120_cfg.h&lt;/STRONG&gt; or you can create your own file, e.g. &lt;STRONG&gt;My_K70_Board_cfg.h&lt;/STRONG&gt;. Just make sure the file matches your board schematic (UART channel, UART pins and GPIO pin if needed).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-&amp;nbsp;&amp;nbsp;&amp;nbsp; You are correct that &lt;STRONG&gt;FSL_Kinetis_Bootloader&lt;/STRONG&gt; only supports K64 right now, and it is focused in new Kinetis devices, so K70 has to wait.&lt;/P&gt;&lt;P&gt;-&amp;nbsp;&amp;nbsp;&amp;nbsp; There are some other application notes about Kinetis bootloaders. You may want to give them a check: &lt;STRONG&gt;AN4367&lt;/STRONG&gt;, &lt;STRONG&gt;AN4368&lt;/STRONG&gt;, &lt;STRONG&gt;AN4370&lt;/STRONG&gt;, &lt;STRONG&gt;AN4379&lt;/STRONG&gt;, &lt;STRONG&gt;AN4764&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; &lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Aug 2014 21:25:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-program-K70-flash-via-USB/m-p/384844#M20667</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2014-08-27T21:25:39Z</dc:date>
    </item>
    <item>
      <title>Re: How to program K70 flash via USB ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-program-K70-flash-via-USB/m-p/384845#M20668</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can get boot loaders for the K70 from &lt;A href="http://www.utasker.com/kinetis.html" title="http://www.utasker.com/kinetis.html"&gt;http://www.utasker.com/kinetis.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;See also &lt;A href="https://community.nxp.com/thread/317301"&gt;Kinetis Boot Loader for SREC UART, SD Card and USB-MSD loading&lt;/A&gt;&lt;/P&gt;&lt;P&gt;This includes USB-HID support for the FSL Kinetis Bootloader PC utility (for all KL and K devices with USB).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Aug 2014 00:01:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-program-K70-flash-via-USB/m-p/384845#M20668</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2014-08-28T00:01:26Z</dc:date>
    </item>
    <item>
      <title>Re: How to program K70 flash via USB ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-program-K70-flash-via-USB/m-p/384846#M20669</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jorge&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;First, thanks a lot !!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Concerning the meaning of:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;But now the extern part of the product is ready, this programation method needs the product to be took to pieces...&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; -&amp;gt; that means I can't easily access the JTAG header connector&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am going to begin by interesting me in the Ezport solution and reading the AN that you suggested me&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="sel" style="background-color: #; color: #;"&gt;I'll keep you posted&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks again&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Sébastien&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Aug 2014 07:16:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-program-K70-flash-via-USB/m-p/384846#M20669</guid>
      <dc:creator>sebastienpeyrau</dc:creator>
      <dc:date>2014-08-28T07:16:33Z</dc:date>
    </item>
    <item>
      <title>Re: How to program K70 flash via USB ?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-program-K70-flash-via-USB/m-p/384847#M20670</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Mark,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks a lot&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am going to look at all this !!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="sel" style="background-color: #; color: #;"&gt;I'll keep you posted&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks again&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Sébastien&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Aug 2014 07:30:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-program-K70-flash-via-USB/m-p/384847#M20670</guid>
      <dc:creator>sebastienpeyrau</dc:creator>
      <dc:date>2014-08-28T07:30:15Z</dc:date>
    </item>
  </channel>
</rss>