<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Two 4 bit SDIO buses on Kinetis K60</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Two-4-bit-SDIO-buses-on-Kinetis-K60/m-p/384516#M20618</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;STRONG style="text-decoration: underline;"&gt;&lt;/STRONG&gt;Alex&lt;/P&gt;&lt;P&gt;This is controlled by the Port Control Module on the K60, which selects which alternate configurations are in use.&amp;nbsp; Those are listed in the Signal Multiplexing and Pin Assignments section in Document &lt;SPAN style="color: #000000; font-family: HelveticaLTStd-Bold; font-size: 20pt; font-style: normal;"&gt;&lt;STRONG&gt;K60P144M120SF3.&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: HelveticaLTStd-Bold; font-size: 20pt; font-style: normal;"&gt;&lt;STRONG&gt;&lt;BR /&gt;&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I looked briefly and I saw only one SDHC assignable in the table. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Good luck,&lt;/P&gt;&lt;P&gt;Larry&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 13 Mar 2015 16:08:36 GMT</pubDate>
    <dc:creator>larryc</dc:creator>
    <dc:date>2015-03-13T16:08:36Z</dc:date>
    <item>
      <title>Two 4 bit SDIO buses on Kinetis K60</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Two-4-bit-SDIO-buses-on-Kinetis-K60/m-p/384515#M20617</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, everyone. I need to use two SDIO bus on the same Kinetis K60 board. One for SD card, another for Wi-Fi module with SDIO interface. Is is t posible to use GPIO as a BUS like SDIO? I want to use SD card in 4 bit mode.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Mar 2015 14:44:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Two-4-bit-SDIO-buses-on-Kinetis-K60/m-p/384515#M20617</guid>
      <dc:creator>alexandersavche</dc:creator>
      <dc:date>2015-03-13T14:44:30Z</dc:date>
    </item>
    <item>
      <title>Re: Two 4 bit SDIO buses on Kinetis K60</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Two-4-bit-SDIO-buses-on-Kinetis-K60/m-p/384516#M20618</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;STRONG style="text-decoration: underline;"&gt;&lt;/STRONG&gt;Alex&lt;/P&gt;&lt;P&gt;This is controlled by the Port Control Module on the K60, which selects which alternate configurations are in use.&amp;nbsp; Those are listed in the Signal Multiplexing and Pin Assignments section in Document &lt;SPAN style="color: #000000; font-family: HelveticaLTStd-Bold; font-size: 20pt; font-style: normal;"&gt;&lt;STRONG&gt;K60P144M120SF3.&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #000000; font-family: HelveticaLTStd-Bold; font-size: 20pt; font-style: normal;"&gt;&lt;STRONG&gt;&lt;BR /&gt;&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I looked briefly and I saw only one SDHC assignable in the table. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Good luck,&lt;/P&gt;&lt;P&gt;Larry&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Mar 2015 16:08:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Two-4-bit-SDIO-buses-on-Kinetis-K60/m-p/384516#M20618</guid>
      <dc:creator>larryc</dc:creator>
      <dc:date>2015-03-13T16:08:36Z</dc:date>
    </item>
    <item>
      <title>Re: Two 4 bit SDIO buses on Kinetis K60</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Two-4-bit-SDIO-buses-on-Kinetis-K60/m-p/384517#M20619</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I saw it. But I want to use one dedicated bus and one additional with free pins (mat be it will software emulated bus).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Mar 2015 08:05:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Two-4-bit-SDIO-buses-on-Kinetis-K60/m-p/384517#M20619</guid>
      <dc:creator>alexandersavche</dc:creator>
      <dc:date>2015-03-16T08:05:58Z</dc:date>
    </item>
    <item>
      <title>Re: Two 4 bit SDIO buses on Kinetis K60</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Two-4-bit-SDIO-buses-on-Kinetis-K60/m-p/384518#M20620</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Alexander Savchencko:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is only one SDHC module in the K60, so you are correct, the solution would be a software emulated bus. I guess you could emulate the SDIO bus by using SPI peripheral. Unfortunately we do not have an example for this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Maybe you can look at the implementation of MSD host from the Freescale USB stack v4.1.1 (download from &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MEDICALUSB&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab" title="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MEDICALUSB&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;USB Stack|Freescale&lt;/A&gt;). The USB MSD example has an option to use SPI interface to talk to an SD card.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;P&gt;Jorge Gonzalez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Mar 2015 00:17:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Two-4-bit-SDIO-buses-on-Kinetis-K60/m-p/384518#M20620</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2015-03-19T00:17:32Z</dc:date>
    </item>
  </channel>
</rss>