<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: USB host communication with more devices</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-host-communication-with-more-devices/m-p/383259#M20445</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Lukas,&lt;/P&gt;&lt;P&gt;I don't think your scheme could achieve.&lt;/P&gt;&lt;P&gt;Selecting a KL or K series MCU as the USB host device can handle the devices whose total number is based on the USB modules the USB host contains under without using the USB HUB.&lt;/P&gt;&lt;P&gt;In another word, if you want to the USB host device communicate with three or more devices, it can't work it out certainly.&lt;/P&gt;&lt;P&gt;Hope the reply helps.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 05 Jan 2015 06:45:57 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2015-01-05T06:45:57Z</dc:date>
    <item>
      <title>USB host communication with more devices</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-host-communication-with-more-devices/m-p/383258#M20444</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I will develop a new project and I need to communicate between one USB host device (maybe Kinetis K or KL) and more devices (8bit MC9S08JS16). Devices will connect to USB host over USB HUB. This is my idea. I haven´t had any experience with USB Stack yet. I need to know if it is possible. Thanks for the answer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Lukas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Jan 2015 10:21:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-host-communication-with-more-devices/m-p/383258#M20444</guid>
      <dc:creator>Luky</dc:creator>
      <dc:date>2015-01-02T10:21:06Z</dc:date>
    </item>
    <item>
      <title>Re: USB host communication with more devices</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-host-communication-with-more-devices/m-p/383259#M20445</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Lukas,&lt;/P&gt;&lt;P&gt;I don't think your scheme could achieve.&lt;/P&gt;&lt;P&gt;Selecting a KL or K series MCU as the USB host device can handle the devices whose total number is based on the USB modules the USB host contains under without using the USB HUB.&lt;/P&gt;&lt;P&gt;In another word, if you want to the USB host device communicate with three or more devices, it can't work it out certainly.&lt;/P&gt;&lt;P&gt;Hope the reply helps.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Jan 2015 06:45:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-host-communication-with-more-devices/m-p/383259#M20445</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2015-01-05T06:45:57Z</dc:date>
    </item>
  </channel>
</rss>