<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックGPIO reset state?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-reset-state/m-p/382780#M20404</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to know the K21 GPIO state during reset.&lt;/P&gt;&lt;P&gt;Where can I find these information?&lt;/P&gt;&lt;P&gt;Could I change the GPIO reset state? If it can be changed, how to do?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 01 Dec 2014 09:12:15 GMT</pubDate>
    <dc:creator>idtericchen</dc:creator>
    <dc:date>2014-12-01T09:12:15Z</dc:date>
    <item>
      <title>GPIO reset state?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-reset-state/m-p/382780#M20404</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to know the K21 GPIO state during reset.&lt;/P&gt;&lt;P&gt;Where can I find these information?&lt;/P&gt;&lt;P&gt;Could I change the GPIO reset state? If it can be changed, how to do?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Dec 2014 09:12:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-reset-state/m-p/382780#M20404</guid>
      <dc:creator>idtericchen</dc:creator>
      <dc:date>2014-12-01T09:12:15Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO reset state?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-reset-state/m-p/382781#M20405</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Eric Chen:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- For digital-only pins the default state is as DISABLED (high impedance).&lt;/P&gt;&lt;P&gt;- For pins with an analog functionality, those acquire their analog function.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can refer to the chapter "&lt;STRONG&gt;K21 Signal Multiplexing and Pin Assignments&lt;/STRONG&gt;" in the Reference Manual to see which pins are digital, analog or digital + analog.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you mean the value of the GPIO registers out of reset, then that information is in each register description, again in the reference manual. e.g. for the GPIOx_PDOR register:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/47735iF9B34BC191EE2725/image-size/large?v=v2&amp;amp;px=999" title="GPIO_register.png" alt="GPIO_register.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;None of the above behaviors can be changed.&lt;/P&gt;&lt;P&gt;In case you cannot find the reference manual in our webpage, please let me know the full part number of your K21 device.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Dec 2014 16:50:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-reset-state/m-p/382781#M20405</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2014-12-01T16:50:07Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO reset state?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-reset-state/m-p/382782#M20406</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jorge:&lt;/P&gt;&lt;P&gt;Thanks for your quickly response.&lt;/P&gt;&lt;P&gt;You mean the digital-only pins the default state is as DISABLED (high impedance) during reset.&lt;/P&gt;&lt;P&gt;So if I want to control GPIO state is HIGH during reset, I need to add external pull-up resistor on this GPIO, right?&lt;/P&gt;&lt;P&gt;For example, If I want the PTD8 to output HIGH during reset, I need to add external pull-up resistor on PTD8, right?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Dec 2014 01:22:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-reset-state/m-p/382782#M20406</guid>
      <dc:creator>idtericchen</dc:creator>
      <dc:date>2014-12-02T01:22:20Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO reset state?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-reset-state/m-p/382783#M20407</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eric:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You are correct, for a high state in PTD8 during reset you can place a pull-up resistor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;P&gt;Jorge Gonzalez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Dec 2014 02:06:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-reset-state/m-p/382783#M20407</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2014-12-02T02:06:19Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO reset state?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-reset-state/m-p/382784#M20408</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jorge,&lt;/P&gt;&lt;P&gt;- For digital-only pins the default state is as DISABLED (high impedance).&lt;/P&gt;&lt;P&gt;- For pins with an analog functionality, those acquire their analog function.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is the above information for all Kinetis unit? I used MK10DN32VFM5.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Look forward to your kindly answer.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Jan 2015 03:55:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-reset-state/m-p/382784#M20408</guid>
      <dc:creator>王剑翰</dc:creator>
      <dc:date>2015-01-30T03:55:56Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO reset state?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-reset-state/m-p/382785#M20409</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes the same applies for your K10 device and any Kinetis K part.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;P&gt;Jorge Gonzalez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Jan 2015 16:57:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-reset-state/m-p/382785#M20409</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2015-01-30T16:57:37Z</dc:date>
    </item>
  </channel>
</rss>