<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: TWR-SER USB Mini AB female connector change to USB Mini B in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-SER-USB-Mini-AB-female-connector-change-to-USB-Mini-B/m-p/382378#M20362</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks! I was looking around for the adapter cable in the shops around, and had to do some digging in the internet. A look in the article on Wikipedia &lt;A href="http://en.wikipedia.org/wiki/USB#Host_and_device_interface_receptacles"&gt;http://en.wikipedia.org/wiki/USB#Host_and_device_interface_receptacles&lt;/A&gt; suggested that the MiniAB receptacles can be plugged with the MiniB connector cables but since they are deprecated, i found it hard to find a suitable cable. I went back and connected the cable to the board and it did connect. Now the next thing is to find if I can actually use it! :smileysilly: I'd test it with some application and post it!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;SPatel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 08 Apr 2015 12:31:08 GMT</pubDate>
    <dc:creator>sohalpatel</dc:creator>
    <dc:date>2015-04-08T12:31:08Z</dc:date>
    <item>
      <title>TWR-SER USB Mini AB female connector change to USB Mini B</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-SER-USB-Mini-AB-female-connector-change-to-USB-Mini-B/m-p/382376#M20360</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As an amateur electronic hobbyist please be gentle on my limited knowledge, having said that, I do have some programming skills but soldering iron is one thing i would use only in dire need. I am trying to use the USB feature of my Kinetis K60F120M oard &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=TWR-K60F120M"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=TWR-K60F120M&lt;/A&gt;. Now looking at the connector on my TWR-SER &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=TWR-SER&amp;amp;lang_cd=en"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=TWR-SER&amp;amp;lang_cd=en&lt;/A&gt; I failed to find a suitable cable. For my convenience, I would like to replace the USB mini AB type female connector with a more generic USB Mini B type female connector. Can anyone suggest if what I am thinking is feasible in the first place? If so, has anyone tried it? Any suggestions in this topic would be very useful. I seriously don't want to blow away my board.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/50553i9F80F757B4EE14F3/image-size/large?v=v2&amp;amp;px=999" title="USB Mini-B Plug.jpg" alt="USB Mini-B Plug.jpg" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/50338i760997BB2466B4DE/image-size/large?v=v2&amp;amp;px=999" title="USB-miniAB.jpg" alt="USB-miniAB.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Apr 2015 08:15:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-SER-USB-Mini-AB-female-connector-change-to-USB-Mini-B/m-p/382376#M20360</guid>
      <dc:creator>sohalpatel</dc:creator>
      <dc:date>2015-04-07T08:15:16Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-SER USB Mini AB female connector change to USB Mini B</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-SER-USB-Mini-AB-female-connector-change-to-USB-Mini-B/m-p/382377#M20361</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sohalpatel,&lt;/P&gt;&lt;P&gt;I think Googling "usb adapter" is safer approach then hardware modifications.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Apr 2015 13:16:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-SER-USB-Mini-AB-female-connector-change-to-USB-Mini-B/m-p/382377#M20361</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2015-04-07T13:16:55Z</dc:date>
    </item>
    <item>
      <title>Re: TWR-SER USB Mini AB female connector change to USB Mini B</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-SER-USB-Mini-AB-female-connector-change-to-USB-Mini-B/m-p/382378#M20362</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks! I was looking around for the adapter cable in the shops around, and had to do some digging in the internet. A look in the article on Wikipedia &lt;A href="http://en.wikipedia.org/wiki/USB#Host_and_device_interface_receptacles"&gt;http://en.wikipedia.org/wiki/USB#Host_and_device_interface_receptacles&lt;/A&gt; suggested that the MiniAB receptacles can be plugged with the MiniB connector cables but since they are deprecated, i found it hard to find a suitable cable. I went back and connected the cable to the board and it did connect. Now the next thing is to find if I can actually use it! :smileysilly: I'd test it with some application and post it!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;SPatel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Apr 2015 12:31:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/TWR-SER-USB-Mini-AB-female-connector-change-to-USB-Mini-B/m-p/382378#M20362</guid>
      <dc:creator>sohalpatel</dc:creator>
      <dc:date>2015-04-08T12:31:08Z</dc:date>
    </item>
  </channel>
</rss>