<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: K30 Input port current consumptions</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K30-Input-port-current-consumptions/m-p/382344#M20358</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Don't let your digital pins float between Vil and Vih -- keep them at valid 'low' or 'high' levels during battery operation.&amp;nbsp; There are discussions elsewhere regarding the blatant error in the datasheets regarding the 'high state' measurement point of Vdd versus Vih.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 27 Aug 2014 21:21:36 GMT</pubDate>
    <dc:creator>egoodii</dc:creator>
    <dc:date>2014-08-27T21:21:36Z</dc:date>
    <item>
      <title>K30 Input port current consumptions</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K30-Input-port-current-consumptions/m-p/382342#M20356</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have a plan to use K30 in our battery powered application.&lt;/P&gt;&lt;P&gt;I was going through K30P144M100SF2V2 Device datasheet and I got shocked when I saw below tables.&lt;/P&gt;&lt;P&gt;These values are meaninglessly very high for a battery powered application.&lt;/P&gt;&lt;P&gt;Is there a chance that datasheet values are wrong?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was relying on stop3 mode power consumption which is around 3uA.&lt;/P&gt;&lt;P&gt;But what is the benefit of low leakage stop modes while MCU consumes more from its digital inputs? &lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/44733i73630AF20321EA4D/image-size/large?v=v2&amp;amp;px=999" title="K30.png" alt="K30.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Aug 2014 14:04:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K30-Input-port-current-consumptions/m-p/382342#M20356</guid>
      <dc:creator>BasePointer</dc:creator>
      <dc:date>2014-08-26T14:04:57Z</dc:date>
    </item>
    <item>
      <title>Re: K30 Input port current consumptions</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K30-Input-port-current-consumptions/m-p/382343#M20357</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That is why you use a Kinetis KL for battery powered applications and not a Kinetis K, most preferreably a device in a WLCSP package. egarding the datasheet power figures, they are correct.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Aug 2014 17:28:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K30-Input-port-current-consumptions/m-p/382343#M20357</guid>
      <dc:creator>apanecatl</dc:creator>
      <dc:date>2014-08-27T17:28:57Z</dc:date>
    </item>
    <item>
      <title>Re: K30 Input port current consumptions</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K30-Input-port-current-consumptions/m-p/382344#M20358</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Don't let your digital pins float between Vil and Vih -- keep them at valid 'low' or 'high' levels during battery operation.&amp;nbsp; There are discussions elsewhere regarding the blatant error in the datasheets regarding the 'high state' measurement point of Vdd versus Vih.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Aug 2014 21:21:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K30-Input-port-current-consumptions/m-p/382344#M20358</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2014-08-27T21:21:36Z</dc:date>
    </item>
    <item>
      <title>Re: K30 Input port current consumptions</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K30-Input-port-current-consumptions/m-p/382345#M20359</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, the application is not always battery powered. Sometimes it takes the power from main supply and we need some M4 DSP functionality there, this is the reason K series is required.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Aug 2014 10:46:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K30-Input-port-current-consumptions/m-p/382345#M20359</guid>
      <dc:creator>BasePointer</dc:creator>
      <dc:date>2014-08-28T10:46:22Z</dc:date>
    </item>
  </channel>
</rss>