<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Kinetis Bootloader - porting project to uVision in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-Bootloader-porting-project-to-uVision/m-p/382244#M20355</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN&gt;Hi Johntt, I'd like to suggest that you can give a check to AN2295 which includes projects for Keil uVision. This bootloader uses a serial UART interface. You can also refer to the post about the step of porting a bootloader project to Keil uVision. Please get the more information through the two links as follow. &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="http://cache.freescale.com/files/microcontrollers/doc/app_note/AN2295.pdf"&gt;http://cache.freescale.com/files/microcontrollers/doc/app_note/AN2295.pdf&lt;/A&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;A _jive_internal="true" data-containerid="2023" data-containertype="14" data-objectid="338822" data-objecttype="2" href="https://community.nxp.com/message/338822#338822"&gt;https://community.freescale.com/message/338822#338822&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 04 Jan 2015 07:30:47 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2015-01-04T07:30:47Z</dc:date>
    <item>
      <title>Kinetis Bootloader - porting project to uVision</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-Bootloader-porting-project-to-uVision/m-p/382243#M20354</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm trying to port Kinetis Bootloader project from IAR Embedded Workbench to Keil uVision, but unfortunately I've got stuck while working with linker things. There is some declaration of data_rom_end variable in startup.c file but I don't know what to set, because Image$$RO$Limit is undefined (Image$$RO$$Base works). Instead of using KEIL and __CC_ARM definitions I've put __ICCARM__ in C/C++ compiler options. Did anyone got success with porting Kinetis Bootloader to uVision?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Jan 2015 05:29:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-Bootloader-porting-project-to-uVision/m-p/382243#M20354</guid>
      <dc:creator>johntt</dc:creator>
      <dc:date>2015-01-01T05:29:53Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis Bootloader - porting project to uVision</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-Bootloader-porting-project-to-uVision/m-p/382244#M20355</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN&gt;Hi Johntt, I'd like to suggest that you can give a check to AN2295 which includes projects for Keil uVision. This bootloader uses a serial UART interface. You can also refer to the post about the step of porting a bootloader project to Keil uVision. Please get the more information through the two links as follow. &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="http://cache.freescale.com/files/microcontrollers/doc/app_note/AN2295.pdf"&gt;http://cache.freescale.com/files/microcontrollers/doc/app_note/AN2295.pdf&lt;/A&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;A _jive_internal="true" data-containerid="2023" data-containertype="14" data-objectid="338822" data-objecttype="2" href="https://community.nxp.com/message/338822#338822"&gt;https://community.freescale.com/message/338822#338822&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 04 Jan 2015 07:30:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-Bootloader-porting-project-to-uVision/m-p/382244#M20355</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2015-01-04T07:30:47Z</dc:date>
    </item>
  </channel>
</rss>