<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックJ199 labels are misleading on FRDM-K64F Quick Reference Card</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/J199-labels-are-misleading-on-FRDM-K64F-Quick-Reference-Card/m-p/381752#M20308</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;FYI the pin labels are next to the wrong pins for J199 on the Quick Reference Card for the FRDM-K64F.&lt;/P&gt;&lt;P&gt;This is the red &amp;amp; white card that comes as part of the packaging for the Freedom board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The J199 connector is shown in one image (Figure 1) with an arrow pointing to it from a label "Add-on BT Module JY-MCU BT Board V1.05"&lt;/P&gt;&lt;P&gt;The other image (Figure 2) shows labels for each pin (1-P3V3, 2-GND, 3-PTC14, 4-PTC15) but the label for pin 1 is next to pin 4 and vice-versa.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 17 Feb 2015 22:06:46 GMT</pubDate>
    <dc:creator>dougturnbow</dc:creator>
    <dc:date>2015-02-17T22:06:46Z</dc:date>
    <item>
      <title>J199 labels are misleading on FRDM-K64F Quick Reference Card</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/J199-labels-are-misleading-on-FRDM-K64F-Quick-Reference-Card/m-p/381752#M20308</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;FYI the pin labels are next to the wrong pins for J199 on the Quick Reference Card for the FRDM-K64F.&lt;/P&gt;&lt;P&gt;This is the red &amp;amp; white card that comes as part of the packaging for the Freedom board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The J199 connector is shown in one image (Figure 1) with an arrow pointing to it from a label "Add-on BT Module JY-MCU BT Board V1.05"&lt;/P&gt;&lt;P&gt;The other image (Figure 2) shows labels for each pin (1-P3V3, 2-GND, 3-PTC14, 4-PTC15) but the label for pin 1 is next to pin 4 and vice-versa.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Feb 2015 22:06:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/J199-labels-are-misleading-on-FRDM-K64F-Quick-Reference-Card/m-p/381752#M20308</guid>
      <dc:creator>dougturnbow</dc:creator>
      <dc:date>2015-02-17T22:06:46Z</dc:date>
    </item>
    <item>
      <title>Re: J199 labels are misleading on FRDM-K64F Quick Reference Card</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/J199-labels-are-misleading-on-FRDM-K64F-Quick-Reference-Card/m-p/381753#M20309</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Doug:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You are right, the J199 header numbers are mirrored in that card. We apologize for this inconvenience, which could cause connection problems.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your observation, I will communicate it to the proper marketing team.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;P&gt;Jorge Gonzalez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Feb 2015 02:05:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/J199-labels-are-misleading-on-FRDM-K64F-Quick-Reference-Card/m-p/381753#M20309</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2015-02-24T02:05:59Z</dc:date>
    </item>
  </channel>
</rss>