<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: GPIO pin as interrupt source</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-pin-as-interrupt-source/m-p/381676#M20305</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you have a GPIO configured to generate an interrupt on a falling or rising edge (eg. PORTC_PCR8 is originally 0x000a0103 for falling edge sensitive interrupt with pull-up enabled) you can change its direction from input to output (in GPIOC_PDDR bit 0 to 1) and it will drive the value in GPIOC_PDOR to the pin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;At the same time each change of the pin value from '1' to '0' will still trigger the original falling edge interrupt.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This allows generating a port interrupt by controlling the value on a GPIO output pin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 06 Nov 2014 02:25:55 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2014-11-06T02:25:55Z</dc:date>
    <item>
      <title>GPIO pin as interrupt source</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-pin-as-interrupt-source/m-p/381674#M20303</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi-&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The mode i am using is MK20DX256VMX7. I have a GPIO pin PTC8 initially set as input and interrupt source. If I change the pin later in code to toggling as code below, will it trigger interrupt?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;/* testing on PTC8: turn off the GPIO */&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;PORT_PCR_REG(PORTC_BASE_PTR, 8) = PORT_PCR_MUX(0x01);&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;GPIO_PDDR_REG(PTC_BASE_PTR) |= 1 &amp;lt;&amp;lt; 8; // PTC8 as output&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;GPIO_PDOR_REG(PTC_BASE_PTR) |= (1 &amp;lt;&amp;lt; 8); // PTC8 in high level&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;_time_delay(10);&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;/* testing on PTC8: turn off the GPIO */&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;PORT_PCR_REG(PORTC_BASE_PTR, 8) = PORT_PCR_MUX(0x01);&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;GPIO_PDDR_REG(PTC_BASE_PTR) |= 1 &amp;lt;&amp;lt; 8; // PTC8 as output&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;GPIO_PDOR_REG(PTC_BASE_PTR) &amp;amp;= ~(1 &amp;lt;&amp;lt; 8); // PTC8 in low level&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;_time_delay(10)&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hui&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Nov 2014 01:20:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-pin-as-interrupt-source/m-p/381674#M20303</guid>
      <dc:creator>huishao2</dc:creator>
      <dc:date>2014-11-06T01:20:42Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO pin as interrupt source</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-pin-as-interrupt-source/m-p/381675#M20304</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hui,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have you config the IRQC:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/45760i1C464ECE97A64FE2/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and config the corresponding interrupt vector table ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;ALice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Nov 2014 01:50:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-pin-as-interrupt-source/m-p/381675#M20304</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2014-11-06T01:50:55Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO pin as interrupt source</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-pin-as-interrupt-source/m-p/381676#M20305</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you have a GPIO configured to generate an interrupt on a falling or rising edge (eg. PORTC_PCR8 is originally 0x000a0103 for falling edge sensitive interrupt with pull-up enabled) you can change its direction from input to output (in GPIOC_PDDR bit 0 to 1) and it will drive the value in GPIOC_PDOR to the pin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;At the same time each change of the pin value from '1' to '0' will still trigger the original falling edge interrupt.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This allows generating a port interrupt by controlling the value on a GPIO output pin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Nov 2014 02:25:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-pin-as-interrupt-source/m-p/381676#M20305</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2014-11-06T02:25:55Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO pin as interrupt source</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-pin-as-interrupt-source/m-p/381677#M20306</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot for your reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hui&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Nov 2014 04:56:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-pin-as-interrupt-source/m-p/381677#M20306</guid>
      <dc:creator>huishao2</dc:creator>
      <dc:date>2014-11-06T04:56:30Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO pin as interrupt source</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-pin-as-interrupt-source/m-p/381678#M20307</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alice&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you so much for your help!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hui&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Nov 2014 04:57:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/GPIO-pin-as-interrupt-source/m-p/381678#M20307</guid>
      <dc:creator>huishao2</dc:creator>
      <dc:date>2014-11-06T04:57:58Z</dc:date>
    </item>
  </channel>
</rss>