<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: QEI inputs</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/QEI-inputs/m-p/150564#M203</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;See K-40 Series, With Flex timer peripheral.&lt;/P&gt;&lt;P&gt;Has option to Quadrature Decoder mode&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 23 Sep 2012 09:39:45 GMT</pubDate>
    <dc:creator>mf_kappa</dc:creator>
    <dc:date>2012-09-23T09:39:45Z</dc:date>
    <item>
      <title>QEI inputs</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/QEI-inputs/m-p/150563#M202</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I´m looking for a Kinetis with quadrature encoder input.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;None found. Is it correct&amp;nbsp; ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Apr 2012 06:15:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/QEI-inputs/m-p/150563#M202</guid>
      <dc:creator>marcelo_freek</dc:creator>
      <dc:date>2012-04-02T06:15:10Z</dc:date>
    </item>
    <item>
      <title>Re: QEI inputs</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/QEI-inputs/m-p/150564#M203</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;See K-40 Series, With Flex timer peripheral.&lt;/P&gt;&lt;P&gt;Has option to Quadrature Decoder mode&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 23 Sep 2012 09:39:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/QEI-inputs/m-p/150564#M203</guid>
      <dc:creator>mf_kappa</dc:creator>
      <dc:date>2012-09-23T09:39:45Z</dc:date>
    </item>
    <item>
      <title>Re: QEI inputs</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/QEI-inputs/m-p/150565#M204</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;All the kinetis microcontrollers feature one or more FlexTimers (FTM) which supports Quadrature decoder with input filters, relative position counting, and interrupt on position count or capture of position count on external event&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Oct 2012 15:48:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/QEI-inputs/m-p/150565#M204</guid>
      <dc:creator>apanecatl</dc:creator>
      <dc:date>2012-10-22T15:48:10Z</dc:date>
    </item>
    <item>
      <title>Re: QEI inputs</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/QEI-inputs/m-p/150566#M205</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Just one problem with that answer - it is not correct. Not all Kinetis MCUs have a an FTM. &lt;/P&gt;&lt;P&gt;It seems you are not the only one with this mistaken notion. On the Freedom Board they pinned it out as FTM, when in fact it is TPM.&lt;/P&gt;&lt;P&gt;Example:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The KL25 Has a TPM, quoting from the RM:&lt;/P&gt;&lt;P&gt;(Document Number: KL25P80M48SF0RM)&lt;/P&gt;&lt;P&gt;"The TPM is built upon a very simple timer (HCS08 Timer PWM Module – TPM) used&lt;/P&gt;&lt;P&gt;for many years on Freescale's 8-bit microcontrollers. The TPM extends the functionality&lt;/P&gt;&lt;P&gt;to support operation in low power modes by clocking the counter, compare and capture&lt;/P&gt;&lt;P&gt;registers from an asynchronous clock that can remain functional in low power modes"&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Oct 2012 12:14:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/QEI-inputs/m-p/150566#M205</guid>
      <dc:creator>JimDon</dc:creator>
      <dc:date>2012-10-23T12:14:38Z</dc:date>
    </item>
    <item>
      <title>Re: QEI inputs</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/QEI-inputs/m-p/150567#M206</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I forgot to mention I was referring to the K family&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Oct 2012 13:42:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/QEI-inputs/m-p/150567#M206</guid>
      <dc:creator>apanecatl</dc:creator>
      <dc:date>2012-10-23T13:42:17Z</dc:date>
    </item>
  </channel>
</rss>