<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Which Kinetis series microcontrollers can be programmed using FRDM-K20D50M Board?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-Kinetis-series-microcontrollers-can-be-programmed-using/m-p/381431#M20295</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;As per the documentation if i m correct, OpenSDAV2 Supports different hardware but it don't work with Code Warrior?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Amit&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 05 Jan 2015 07:15:52 GMT</pubDate>
    <dc:creator>Amit_Kumar1</dc:creator>
    <dc:date>2015-01-05T07:15:52Z</dc:date>
    <item>
      <title>Which Kinetis series microcontrollers can be programmed using FRDM-K20D50M Board?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-Kinetis-series-microcontrollers-can-be-programmed-using/m-p/381428#M20292</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to know which uc can be programmed using Open SDA? I would be making custom boards with new (factory) programmed microcontrollers. Is there any way I can use onboard OpenSDA to program new uc? If This issue is cleared then many new learners can use freescale for low cost product development. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind Regards&lt;/P&gt;&lt;P&gt;Amit&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Dec 2014 06:10:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-Kinetis-series-microcontrollers-can-be-programmed-using/m-p/381428#M20292</guid>
      <dc:creator>Amit_Kumar1</dc:creator>
      <dc:date>2014-12-31T06:10:52Z</dc:date>
    </item>
    <item>
      <title>Re: Which Kinetis series microcontrollers can be programmed using FRDM-K20D50M Board?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-Kinetis-series-microcontrollers-can-be-programmed-using/m-p/381429#M20293</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I Think we cannot directly use open SDA for other uc we would be needing to change the open SDA to USBDM my changing bootloader. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Jan 2015 08:04:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-Kinetis-series-microcontrollers-can-be-programmed-using/m-p/381429#M20293</guid>
      <dc:creator>Amit_Kumar1</dc:creator>
      <dc:date>2015-01-02T08:04:47Z</dc:date>
    </item>
    <item>
      <title>Re: Which Kinetis series microcontrollers can be programmed using FRDM-K20D50M Board?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-Kinetis-series-microcontrollers-can-be-programmed-using/m-p/381430#M20294</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Amit,&lt;/P&gt;&lt;P&gt;The OpenSDA interface in the FRDM-K20D50M board only support to program the K20, it will fail to program the other MCU.&lt;/P&gt;&lt;P&gt;However FSL already provided another version of the OpenSDA, I think it could meet your needs.&lt;/P&gt;&lt;P&gt;Please get the more detail information about the OpenSDA interface through the link as follow.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-100720"&gt;OpenSDAv2&lt;/A&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 04 Jan 2015 06:53:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-Kinetis-series-microcontrollers-can-be-programmed-using/m-p/381430#M20294</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2015-01-04T06:53:28Z</dc:date>
    </item>
    <item>
      <title>Re: Which Kinetis series microcontrollers can be programmed using FRDM-K20D50M Board?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-Kinetis-series-microcontrollers-can-be-programmed-using/m-p/381431#M20295</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;As per the documentation if i m correct, OpenSDAV2 Supports different hardware but it don't work with Code Warrior?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Amit&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Jan 2015 07:15:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-Kinetis-series-microcontrollers-can-be-programmed-using/m-p/381431#M20295</guid>
      <dc:creator>Amit_Kumar1</dc:creator>
      <dc:date>2015-01-05T07:15:52Z</dc:date>
    </item>
    <item>
      <title>Re: Which Kinetis series microcontrollers can be programmed using FRDM-K20D50M Board?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-Kinetis-series-microcontrollers-can-be-programmed-using/m-p/381432#M20296</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Amit,&lt;/P&gt;&lt;P&gt;100% right.&lt;/P&gt;&lt;P&gt;The updated KDS could work well with the OpenSDA2, you can use it instead of the Code warrior.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Jan 2015 08:04:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-Kinetis-series-microcontrollers-can-be-programmed-using/m-p/381432#M20296</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2015-01-05T08:04:38Z</dc:date>
    </item>
  </channel>
</rss>