<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 MKL26Z64 m_text overflow using CMSIS DSP Library</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL26Z64-m-text-overflow-using-CMSIS-DSP-Library/m-p/380953#M20248</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi. I'm developing an application for a custom board using MKL26Z64. The application involves an FFT. To do so, I included the CMSIS DSP Library.&lt;/P&gt;&lt;P&gt;However, when I use the arm_rfft_init_q15 and arm_rfft_q15 functions to perform a fixed-point real FFT, the code (which was 8384 bytes before) overflows by 23124 bytes. When I remove those functions, there's no overflow.&lt;/P&gt;&lt;P&gt;I'm using CodeWarrior 10.6 and Processor Expert 10.3.&lt;/P&gt;&lt;P&gt;Any tips on this? Do I have to use another FFT implementation?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 29 Nov 2014 21:32:30 GMT</pubDate>
    <dc:creator>gustavsl</dc:creator>
    <dc:date>2014-11-29T21:32:30Z</dc:date>
    <item>
      <title>MKL26Z64 m_text overflow using CMSIS DSP Library</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL26Z64-m-text-overflow-using-CMSIS-DSP-Library/m-p/380953#M20248</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi. I'm developing an application for a custom board using MKL26Z64. The application involves an FFT. To do so, I included the CMSIS DSP Library.&lt;/P&gt;&lt;P&gt;However, when I use the arm_rfft_init_q15 and arm_rfft_q15 functions to perform a fixed-point real FFT, the code (which was 8384 bytes before) overflows by 23124 bytes. When I remove those functions, there's no overflow.&lt;/P&gt;&lt;P&gt;I'm using CodeWarrior 10.6 and Processor Expert 10.3.&lt;/P&gt;&lt;P&gt;Any tips on this? Do I have to use another FFT implementation?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 29 Nov 2014 21:32:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL26Z64-m-text-overflow-using-CMSIS-DSP-Library/m-p/380953#M20248</guid>
      <dc:creator>gustavsl</dc:creator>
      <dc:date>2014-11-29T21:32:30Z</dc:date>
    </item>
    <item>
      <title>Re: MKL26Z64 m_text overflow using CMSIS DSP Library</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL26Z64-m-text-overflow-using-CMSIS-DSP-Library/m-p/380954#M20249</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Gustavo Leal:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Check the next thread and especially the Correct Answer by colleague Martyn Hunt. Maybe your project is linking the whole DSP library and you have to use the &lt;SPAN style="color: #1f497d;"&gt;-ffunction-sections -fdata-sections&lt;/SPAN&gt; compiler options:&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;&lt;A href="https://community.nxp.com/message/414791"&gt;Has anybody implemented CMSIS FFT library Successfully?&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Dec 2014 02:09:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL26Z64-m-text-overflow-using-CMSIS-DSP-Library/m-p/380954#M20249</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2014-12-01T02:09:26Z</dc:date>
    </item>
  </channel>
</rss>