<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Incorrect DDR2 configuration in TOWER defaults</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Incorrect-DDR2-configuration-in-TOWER-defaults/m-p/380394#M20207</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;K70 DDR2 Controller only support single-ended DQS. As I check TWR-K70F120M board DDR2 initialization code with below setting about DDR_CR21:&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;DDR_CR21 = 0x00040232;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;So, the DDR2 memory still keep the default DQS# setting, which default is disable.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;BR /&gt;best regards &lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 27 Aug 2014 06:37:52 GMT</pubDate>
    <dc:creator>Hui_Ma</dc:creator>
    <dc:date>2014-08-27T06:37:52Z</dc:date>
    <item>
      <title>Incorrect DDR2 configuration in TOWER defaults</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Incorrect-DDR2-configuration-in-TOWER-defaults/m-p/380393#M20206</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The default DDR configuration for the tower project sets&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; DDR_CR21 = 0x20040232&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;More specifically it clears MR1DAT0 bit E11, which means that DQS# is enabled (See DDR UM: EMR definition). This is incorrect since the Kinetis DRAM controller &lt;SPAN style="text-decoration: underline;"&gt;only supports single-ended DQS&lt;/SPAN&gt;. Right??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm extremely surprised no one else has mentioned this in the community, probably due to the extremely poor documentation of the DRAM controller so people just give up.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Aug 2014 23:36:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Incorrect-DDR2-configuration-in-TOWER-defaults/m-p/380393#M20206</guid>
      <dc:creator>bjoernjohanness</dc:creator>
      <dc:date>2014-08-25T23:36:43Z</dc:date>
    </item>
    <item>
      <title>Re: Incorrect DDR2 configuration in TOWER defaults</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Incorrect-DDR2-configuration-in-TOWER-defaults/m-p/380394#M20207</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;K70 DDR2 Controller only support single-ended DQS. As I check TWR-K70F120M board DDR2 initialization code with below setting about DDR_CR21:&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;DDR_CR21 = 0x00040232;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;So, the DDR2 memory still keep the default DQS# setting, which default is disable.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;BR /&gt;best regards &lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Aug 2014 06:37:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Incorrect-DDR2-configuration-in-TOWER-defaults/m-p/380394#M20207</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2014-08-27T06:37:52Z</dc:date>
    </item>
    <item>
      <title>Re: Incorrect DDR2 configuration in TOWER defaults</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Incorrect-DDR2-configuration-in-TOWER-defaults/m-p/380395#M20208</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ma, thank you for your reply. I appreciate it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please take a second to elaborate how you reach that conclusion? Which of the 32 bits in 0x00040232 will keep the DDR2 memory in it's "default DQS# setting"?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;//bjoern&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Aug 2014 16:39:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Incorrect-DDR2-configuration-in-TOWER-defaults/m-p/380395#M20208</guid>
      <dc:creator>bjoernjohanness</dc:creator>
      <dc:date>2014-08-27T16:39:44Z</dc:date>
    </item>
    <item>
      <title>Re: Re: Incorrect DDR2 configuration in TOWER defaults</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Incorrect-DDR2-configuration-in-TOWER-defaults/m-p/380396#M20209</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Update: Since Ma Hui has no interest in replying with the correct answer, I'll provide it to whoever is interested:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As mentioned, turns out that the TOWER project ("K70 DDR2 configuration tool" etc.) is incorrectly configured. Freescale now acknowledges this.&lt;STRONG&gt; Bit E10 in EMR1 should be SET&lt;/STRONG&gt; rather than cleared in order to disable DQS#, which physically isn't supported by Kinetis. Hence, something like this is in order:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;DDR_CR21 = 0x20040232&amp;nbsp; |&amp;nbsp; (1 &amp;lt;&amp;lt; (10+16) );&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Sep 2014 21:09:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Incorrect-DDR2-configuration-in-TOWER-defaults/m-p/380396#M20209</guid>
      <dc:creator>bjoernjohanness</dc:creator>
      <dc:date>2014-09-15T21:09:17Z</dc:date>
    </item>
  </channel>
</rss>