<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Accuracy specs of the K64_120 on board RTC</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Accuracy-specs-of-the-K64-120-on-board-RTC/m-p/379792#M20164</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The K64 RTC is just a counter -- accuracy is entirely up to the crystal specs and as tuned with the onchip caps.&amp;nbsp; I get about 1sec/day (11.6ppm).&amp;nbsp; You can 'do better' compensating for TC, but 'only while the CPU is running' (say you wake up every hour and adjust the caps OR the 'compensation reg').&amp;nbsp; I don't use the compensation reg, mostly because I am extrapolating the prescaler counts to time 'tens of microseconds' at the lowest level, and that math requires 32768 counts per second.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My XTAL = Abracon ABS10-32.768KHZ-7-T&amp;nbsp;&amp;nbsp;&amp;nbsp; +/-20ppm, another 0 to -20ppm 10C to 50C&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I set the chip caps to 8 pf.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 25 Aug 2014 18:25:43 GMT</pubDate>
    <dc:creator>egoodii</dc:creator>
    <dc:date>2014-08-25T18:25:43Z</dc:date>
    <item>
      <title>Accuracy specs of the K64_120 on board RTC</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Accuracy-specs-of-the-K64-120-on-board-RTC/m-p/379791#M20163</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I can't seem to find any specs on the accuracy of the RTC built into the K64_120.&amp;nbsp; Is it 1 sec/year or 1 sec/day or somewhere in between.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you know of a doc that can clue me in I would much appreciate.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for any info you can provide!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Aug 2014 18:05:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Accuracy-specs-of-the-K64-120-on-board-RTC/m-p/379791#M20163</guid>
      <dc:creator>tim</dc:creator>
      <dc:date>2014-08-25T18:05:36Z</dc:date>
    </item>
    <item>
      <title>Re: Accuracy specs of the K64_120 on board RTC</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Accuracy-specs-of-the-K64-120-on-board-RTC/m-p/379792#M20164</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The K64 RTC is just a counter -- accuracy is entirely up to the crystal specs and as tuned with the onchip caps.&amp;nbsp; I get about 1sec/day (11.6ppm).&amp;nbsp; You can 'do better' compensating for TC, but 'only while the CPU is running' (say you wake up every hour and adjust the caps OR the 'compensation reg').&amp;nbsp; I don't use the compensation reg, mostly because I am extrapolating the prescaler counts to time 'tens of microseconds' at the lowest level, and that math requires 32768 counts per second.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My XTAL = Abracon ABS10-32.768KHZ-7-T&amp;nbsp;&amp;nbsp;&amp;nbsp; +/-20ppm, another 0 to -20ppm 10C to 50C&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I set the chip caps to 8 pf.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Aug 2014 18:25:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Accuracy-specs-of-the-K64-120-on-board-RTC/m-p/379792#M20164</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2014-08-25T18:25:43Z</dc:date>
    </item>
  </channel>
</rss>