<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Single I2S connection to 4 channel DAC in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Single-I2S-connection-to-4-channel-DAC/m-p/379606#M20142</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I'm trying to use the I2S to drive a 4 channel 24 bit DAC.&amp;nbsp; I'm a bit confused as to how the I2S functions on the K20 as it doesn't have a LRCLK and instead has 2 data output pins.&amp;nbsp; Do these represent L/R instead of being time multiplexed or do they both hold L/R giving me 4 channels?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 28 Nov 2014 10:19:35 GMT</pubDate>
    <dc:creator>logangardner</dc:creator>
    <dc:date>2014-11-28T10:19:35Z</dc:date>
    <item>
      <title>Single I2S connection to 4 channel DAC</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Single-I2S-connection-to-4-channel-DAC/m-p/379606#M20142</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I'm trying to use the I2S to drive a 4 channel 24 bit DAC.&amp;nbsp; I'm a bit confused as to how the I2S functions on the K20 as it doesn't have a LRCLK and instead has 2 data output pins.&amp;nbsp; Do these represent L/R instead of being time multiplexed or do they both hold L/R giving me 4 channels?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Nov 2014 10:19:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Single-I2S-connection-to-4-channel-DAC/m-p/379606#M20142</guid>
      <dc:creator>logangardner</dc:creator>
      <dc:date>2014-11-28T10:19:35Z</dc:date>
    </item>
    <item>
      <title>Re: Single I2S connection to 4 channel DAC</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Single-I2S-connection-to-4-channel-DAC/m-p/379607#M20143</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The K20 each I2S module has two data transmit channels pins and two independent data receive channels pins.&lt;/P&gt;&lt;P&gt;Both data transmit channels can work at the same time. The two I2S modules provides 4 data transmit channels.&lt;/P&gt;&lt;P&gt;So, it could match with customer requirement.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;BR /&gt;best regards &lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Dec 2014 06:59:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Single-I2S-connection-to-4-channel-DAC/m-p/379607#M20143</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2014-12-01T06:59:41Z</dc:date>
    </item>
  </channel>
</rss>