<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MKE04Z8VMJ4 and MULTILINK UNIVERSAL in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKE04Z8VMJ4-and-MULTILINK-UNIVERSAL/m-p/379428#M20127</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a problem and want to see if you can help me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to record a Kinetis uControlador Freescale, the &lt;STRONG&gt;MKE04Z8VWJ4&lt;/STRONG&gt; but am not having success ...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using the recorder "&lt;STRONG&gt;Multilink Universal&lt;/STRONG&gt;", &lt;STRONG&gt;green model&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Following existing development models, connected pins "SWD_DIO, SWD_CLK, Reset, + 5V and GND" to the burner pins.&lt;/P&gt;&lt;P&gt;However the time of recording, it generates error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any limitation on the recorder with the microcontroller model?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 06 Apr 2015 12:08:57 GMT</pubDate>
    <dc:creator>charlesdiogoa_</dc:creator>
    <dc:date>2015-04-06T12:08:57Z</dc:date>
    <item>
      <title>MKE04Z8VMJ4 and MULTILINK UNIVERSAL</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKE04Z8VMJ4-and-MULTILINK-UNIVERSAL/m-p/379428#M20127</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a problem and want to see if you can help me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to record a Kinetis uControlador Freescale, the &lt;STRONG&gt;MKE04Z8VWJ4&lt;/STRONG&gt; but am not having success ...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using the recorder "&lt;STRONG&gt;Multilink Universal&lt;/STRONG&gt;", &lt;STRONG&gt;green model&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Following existing development models, connected pins "SWD_DIO, SWD_CLK, Reset, + 5V and GND" to the burner pins.&lt;/P&gt;&lt;P&gt;However the time of recording, it generates error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any limitation on the recorder with the microcontroller model?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Apr 2015 12:08:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKE04Z8VMJ4-and-MULTILINK-UNIVERSAL/m-p/379428#M20127</guid>
      <dc:creator>charlesdiogoa_</dc:creator>
      <dc:date>2015-04-06T12:08:57Z</dc:date>
    </item>
    <item>
      <title>Re: MKE04Z8VMJ4 and MULTILINK UNIVERSAL</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKE04Z8VMJ4-and-MULTILINK-UNIVERSAL/m-p/379429#M20128</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have just seen that has to do with the NMI pin, cut it because the circuit, I can not write ...&lt;/P&gt;&lt;P&gt;but how can I use this pin?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Apr 2015 18:46:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKE04Z8VMJ4-and-MULTILINK-UNIVERSAL/m-p/379429#M20128</guid>
      <dc:creator>charlesdiogoa_</dc:creator>
      <dc:date>2015-04-06T18:46:56Z</dc:date>
    </item>
    <item>
      <title>Re: MKE04Z8VMJ4 and MULTILINK UNIVERSAL</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKE04Z8VMJ4-and-MULTILINK-UNIVERSAL/m-p/379430#M20129</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The P&amp;amp;E USB Multilink Universal tool provides below Kinetis debug port:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/51018i5C4FC56882C7E209/image-size/large?v=v2&amp;amp;px=999" role="button" title="1.png" alt="1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I checked your attached debugger interface, there without problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The NMI pin is default to NMI function after the MCU POR, and there with internal pullup device enabled when NMI is enabled.&lt;/P&gt;&lt;P&gt;When there with low voltage detected at NMI pin, the NMI related Non-maskable interrupt will be triggered with Vector2 at ARM's NVIC.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;best regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Apr 2015 08:36:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKE04Z8VMJ4-and-MULTILINK-UNIVERSAL/m-p/379430#M20129</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2015-04-07T08:36:43Z</dc:date>
    </item>
    <item>
      <title>Re: MKE04Z8VMJ4 and MULTILINK UNIVERSAL</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKE04Z8VMJ4-and-MULTILINK-UNIVERSAL/m-p/379431#M20130</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;but I want to use this NMI pin as output, how do that?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Apr 2015 11:38:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKE04Z8VMJ4-and-MULTILINK-UNIVERSAL/m-p/379431#M20130</guid>
      <dc:creator>charlesdiogoa_</dc:creator>
      <dc:date>2015-04-07T11:38:55Z</dc:date>
    </item>
    <item>
      <title>Re: MKE04Z8VMJ4 and MULTILINK UNIVERSAL</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKE04Z8VMJ4-and-MULTILINK-UNIVERSAL/m-p/379432#M20131</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It can be used, but you will have to make sure nothing attached to it is pulling the pin low until the NMI can be disabled.&amp;nbsp; The SIM module has the registers to control the NMI function.&amp;nbsp; If you're using Processor Expert, it can be disabled through that.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Apr 2015 13:28:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKE04Z8VMJ4-and-MULTILINK-UNIVERSAL/m-p/379432#M20131</guid>
      <dc:creator>davidsherman</dc:creator>
      <dc:date>2015-04-07T13:28:46Z</dc:date>
    </item>
    <item>
      <title>Re: MKE04Z8VMJ4 and MULTILINK UNIVERSAL</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKE04Z8VMJ4-and-MULTILINK-UNIVERSAL/m-p/379433#M20132</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;this one shows how to map the NMI as GPIO pin with Processor Expert:&lt;/P&gt;&lt;P&gt;&lt;A href="http://mcuoneclipse.com/2014/04/18/pin-muxing-using-the-nmi-pin-as-gpio-pin/" title="http://mcuoneclipse.com/2014/04/18/pin-muxing-using-the-nmi-pin-as-gpio-pin/"&gt;Pin Muxing: Using the NMI Pin as GPIO Pin | MCU on Eclipse&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Apr 2015 16:10:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKE04Z8VMJ4-and-MULTILINK-UNIVERSAL/m-p/379433#M20132</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2015-04-07T16:10:24Z</dc:date>
    </item>
  </channel>
</rss>