<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Re: K70 UART0 using ISO7816 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-UART0-using-ISO7816/m-p/378884#M20085</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Stephanos,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The attachment includes all the source files for this demo, you may run the "make_new_project.exe" in the folder of "KINETIS_120MHZ_SC\build\iar", and create a project named as "iso7816_demo", and then copy and replace all the files in the folder of "KINETIS_120MHZ_SC\src\projects\iso7816_demo" with the attached one.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 03 Dec 2014 02:53:58 GMT</pubDate>
    <dc:creator>Kan_Li</dc:creator>
    <dc:date>2014-12-03T02:53:58Z</dc:date>
    <item>
      <title>K70 UART0 using ISO7816</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-UART0-using-ISO7816/m-p/378879#M20080</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to use uart0 for ISO 7816&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SIM power is connected to GPIO&lt;/P&gt;&lt;P&gt;SIM reset is connected to GPIO&lt;/P&gt;&lt;P&gt;SIM clock is connected to FTM0_3&lt;/P&gt;&lt;P&gt;SIM Data is connected to UART0 TX&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How to initialize uart0 and FTM0_3.&lt;/P&gt;&lt;P&gt;and how to get ATR information.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;please help me&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Nov 2014 07:25:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-UART0-using-ISO7816/m-p/378879#M20080</guid>
      <dc:creator>stephanoschoi</dc:creator>
      <dc:date>2014-11-28T07:25:18Z</dc:date>
    </item>
    <item>
      <title>Re: K70 UART0 using ISO7816</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-UART0-using-ISO7816/m-p/378880#M20081</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Stephanos Choi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please kindly refer to the attached ISO7816 demo for details. It is based on TWR-K70F120M.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Dec 2014 03:23:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-UART0-using-ISO7816/m-p/378880#M20081</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2014-12-01T03:23:25Z</dc:date>
    </item>
    <item>
      <title>Re: K70 UART0 using ISO7816</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-UART0-using-ISO7816/m-p/378881#M20082</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have &lt;SPAN class="undefined"&gt;KINETIS_120MHZ_SC but cannot find the demo.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;where is it in &lt;SPAN class="undefined"&gt;KINETIS_120MHZ_SC?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="undefined"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Dec 2014 05:48:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-UART0-using-ISO7816/m-p/378881#M20082</guid>
      <dc:creator>stephanoschoi</dc:creator>
      <dc:date>2014-12-01T05:48:49Z</dc:date>
    </item>
    <item>
      <title>Re: K70 UART0 using ISO7816</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-UART0-using-ISO7816/m-p/378882#M20083</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I wrote that demo based on &lt;SPAN class="undefined"&gt;KINETIS_120MHZ_SC, so it is not in the released version.. Please kindly refer to the attached &lt;SPAN class="undefined"&gt;KINETIS_120MHZ_SC.7z.zip for details.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Dec 2014 07:06:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-UART0-using-ISO7816/m-p/378882#M20083</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2014-12-01T07:06:42Z</dc:date>
    </item>
    <item>
      <title>Re: K70 UART0 using ISO7816</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-UART0-using-ISO7816/m-p/378883#M20084</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But I cannot down load the file, it is displayed like"&lt;STRONG&gt;Security policy violation detected.&lt;/STRONG&gt; The file has been removed."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please send me the file to e-mail ( &lt;A href="mailto:ylive@paran.com"&gt;ylive@paran.com&lt;/A&gt; ).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a nice day.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Stephanos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Dec 2014 12:43:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-UART0-using-ISO7816/m-p/378883#M20084</guid>
      <dc:creator>stephanoschoi</dc:creator>
      <dc:date>2014-12-01T12:43:38Z</dc:date>
    </item>
    <item>
      <title>Re: Re: K70 UART0 using ISO7816</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-UART0-using-ISO7816/m-p/378884#M20085</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Stephanos,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The attachment includes all the source files for this demo, you may run the "make_new_project.exe" in the folder of "KINETIS_120MHZ_SC\build\iar", and create a project named as "iso7816_demo", and then copy and replace all the files in the folder of "KINETIS_120MHZ_SC\src\projects\iso7816_demo" with the attached one.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Dec 2014 02:53:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-UART0-using-ISO7816/m-p/378884#M20085</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2014-12-03T02:53:58Z</dc:date>
    </item>
  </channel>
</rss>