<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Which Kinetis devices have EzPorts?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-Kinetis-devices-have-EzPorts/m-p/376971#M19851</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Chad,&lt;/P&gt;&lt;P&gt;regarding MKL devices, only KL33, KL34 and KL43 seems to include EzPort.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Yasuhiko Koumoto.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 Mar 2015 11:05:12 GMT</pubDate>
    <dc:creator>yasuhikokoumoto</dc:creator>
    <dc:date>2015-03-12T11:05:12Z</dc:date>
    <item>
      <title>Which Kinetis devices have EzPorts?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-Kinetis-devices-have-EzPorts/m-p/376970#M19850</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am considering a design that uses 2 Kinetis processors and having the Master MCU update the firmware on the second MCU via a spare DSPI port.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Usually this would require a custom boot-loader or implementation of JTAG, but the Ezport looks to simplify this task because its SPI.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to select a small, low power Kinetis that has Ezport using the Parameter search tool on the Freescale website, but there is no column I can see that indicates whether or not the device is equipped with an EzPort.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there a list of devices that have EzPort?&amp;nbsp; &lt;/P&gt;&lt;P&gt;Do any of the MKL ( lower power devices ) have EzPort?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Mar 2015 14:20:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-Kinetis-devices-have-EzPorts/m-p/376970#M19850</guid>
      <dc:creator>chadwilliams</dc:creator>
      <dc:date>2015-03-11T14:20:42Z</dc:date>
    </item>
    <item>
      <title>Re: Which Kinetis devices have EzPorts?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-Kinetis-devices-have-EzPorts/m-p/376971#M19851</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Chad,&lt;/P&gt;&lt;P&gt;regarding MKL devices, only KL33, KL34 and KL43 seems to include EzPort.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Yasuhiko Koumoto.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Mar 2015 11:05:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-Kinetis-devices-have-EzPorts/m-p/376971#M19851</guid>
      <dc:creator>yasuhikokoumoto</dc:creator>
      <dc:date>2015-03-12T11:05:12Z</dc:date>
    </item>
    <item>
      <title>Re: Which Kinetis devices have EzPorts?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-Kinetis-devices-have-EzPorts/m-p/376972#M19852</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Chad Williams:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;All of the parts in the Kinetis K family have EzPort, except for K02, which is an entry level MCU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As for Kinetis L devices, unfortunately none of them have the EzPort interface.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Mar 2015 16:41:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-Kinetis-devices-have-EzPorts/m-p/376972#M19852</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2015-03-12T16:41:29Z</dc:date>
    </item>
  </channel>
</rss>