<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: ERRATA  e6573 of K70 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ERRATA-e6573-of-K70/m-p/376763#M19826</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Puspam,&lt;/P&gt;&lt;P&gt;Actually, I'm not very clearly with your question.&lt;/P&gt;&lt;P&gt;You mentioned that you didn' use the JTAG_TRST pin, was that mean you disable the JTAG_TRST function on PTA3 pin?&lt;/P&gt;&lt;P&gt;So I'd like to confirm that with you ASAP, then I can give you appropriate suggestion for you.&lt;/P&gt;&lt;P&gt;I'm looking forward to your reply.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 05 Nov 2014 02:28:45 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2014-11-05T02:28:45Z</dc:date>
    <item>
      <title>ERRATA  e6573 of K70</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ERRATA-e6573-of-K70/m-p/376762#M19825</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi I was going through the ERRATA for k70 and found it is mentioned "e6573: JTAG: JTAG TDO function on the PTA2 disables the pull resistor".&lt;/P&gt;&lt;P&gt;It is adviced to connect Pull device on TDO pin.&lt;/P&gt;&lt;P&gt;Want to know as i am not using JTAG Reset i.e. JTAG_TRST pin of k70 so is it necessary to Pull TDO pin to high or low,&lt;/P&gt;&lt;P&gt;if yes then with what value of resistor shall i pull it high or low ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note: please mention if TDO pin has to be pulled high or low if at all pull is required&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please reply at earliest&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and regards,&lt;/P&gt;&lt;P&gt;Puspam N&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Nov 2014 09:27:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ERRATA-e6573-of-K70/m-p/376762#M19825</guid>
      <dc:creator>puspamnayak</dc:creator>
      <dc:date>2014-11-04T09:27:37Z</dc:date>
    </item>
    <item>
      <title>Re: ERRATA  e6573 of K70</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ERRATA-e6573-of-K70/m-p/376763#M19826</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Puspam,&lt;/P&gt;&lt;P&gt;Actually, I'm not very clearly with your question.&lt;/P&gt;&lt;P&gt;You mentioned that you didn' use the JTAG_TRST pin, was that mean you disable the JTAG_TRST function on PTA3 pin?&lt;/P&gt;&lt;P&gt;So I'd like to confirm that with you ASAP, then I can give you appropriate suggestion for you.&lt;/P&gt;&lt;P&gt;I'm looking forward to your reply.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Nov 2014 02:28:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ERRATA-e6573-of-K70/m-p/376763#M19826</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2014-11-05T02:28:45Z</dc:date>
    </item>
    <item>
      <title>Re: ERRATA  e6573 of K70</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ERRATA-e6573-of-K70/m-p/376764#M19827</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jeremyzhou,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your response. I am not using JTAG_TRST i.e. JTAG RESET and yes it is disabled for now but yes if required then we will use that in future.&lt;/P&gt;&lt;P&gt;So from ERRATA what i understood is that if we are using JTAG_TRST then we need to use a pull-up or pull-down at TDO pin as workaround&amp;nbsp; so as to avoid increased power consumption.&lt;/P&gt;&lt;P&gt;And also i was referring to Tower board schematic of K70 (TWR-K70F120M-SCH) where there is no pull-up or pull-down at TDO pin so i got confused that if really any pull-up/down is required at TDO pin.&amp;nbsp; If it is required then it should be Pull-Up or Pull-Down and what shall be the value of resistor to be considered.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Request you to correct me if my understanding is wrong as per given data in ERRATA e6573 and suggest me accordingly at earliest&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;Puspam Nayak&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Nov 2014 05:04:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ERRATA-e6573-of-K70/m-p/376764#M19827</guid>
      <dc:creator>puspamnayak</dc:creator>
      <dc:date>2014-11-05T05:04:46Z</dc:date>
    </item>
    <item>
      <title>Re: ERRATA  e6573 of K70</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ERRATA-e6573-of-K70/m-p/376765#M19828</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Puspam,&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;Yes, it's recommended to enable pull-up or pull-dow, or add an exteran pull device or external soruce to the pin when set up the PTA2 as a digital input and left unconnected in the circuit from the errata doc.&lt;/P&gt;&lt;P&gt;However in the TWR-K70F120, PTA2 should be supported to work in JTAG_TDO function and according the JTAG debug interface specification, it's not necessary to add an external resistor to the pin.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jeremy&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Nov 2014 02:15:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ERRATA-e6573-of-K70/m-p/376765#M19828</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2014-11-06T02:15:32Z</dc:date>
    </item>
  </channel>
</rss>