<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: The convinient stepper motor driver for FRDM-KL25Z</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/The-convinient-stepper-motor-driver-for-FRDM-KL25Z/m-p/376657#M19802</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can download the example driver that is used to control the &lt;A href="https://community.nxp.com/docs/DOC-93914"&gt;Freescale Cup Shield for the Freedom KL25Z&lt;/A&gt; which has on board 2 channel Motor Driver ICs (MC33887APVW). It might be helpful. Unfortunately we do not have a code driver for the bipolar stepper motors you are using.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this information can help you&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Adrian Sanchez Cano&lt;BR /&gt;Technical Support Engineer&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Feb 2015 17:05:04 GMT</pubDate>
    <dc:creator>adriancano</dc:creator>
    <dc:date>2015-02-03T17:05:04Z</dc:date>
    <item>
      <title>The convinient stepper motor driver for FRDM-KL25Z</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/The-convinient-stepper-motor-driver-for-FRDM-KL25Z/m-p/376653#M19798</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;i have a KL25Z, which i want to drrive multiple stepper motors with.&amp;nbsp; My issue is i need to get a steppper driver that does not need a volt- level shifter. Am requesting if sm1 has tried this out , and what driver can u recommend. I dont want an arduino shien. i need something like a DRV8825. Any help please?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Jan 2015 11:51:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/The-convinient-stepper-motor-driver-for-FRDM-KL25Z/m-p/376653#M19798</guid>
      <dc:creator>kevinamadiva</dc:creator>
      <dc:date>2015-01-26T11:51:57Z</dc:date>
    </item>
    <item>
      <title>Re: The convinient stepper motor driver for FRDM-KL25Z</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/The-convinient-stepper-motor-driver-for-FRDM-KL25Z/m-p/376654#M19799</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Helloo Kevin, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope you are doing great. I have a question, do you need a driver that doesn´t have a level shifter, so the integrated circuit driver will have to have an output of the same voltage that the motor requires? I don´t know what the voltage is required for the motor. &lt;/P&gt;&lt;P&gt;Check the different options on&amp;nbsp; the following link: &lt;A href="http://www.freescale.com/webapp/sps/site/homepage.jsp?code=ANALOGHOME" title="http://www.freescale.com/webapp/sps/site/homepage.jsp?code=ANALOGHOME"&gt;http://www.freescale.com/webapp/sps/site/homepage.jsp?code=ANALOGHOME&lt;/A&gt;&lt;/P&gt;&lt;P&gt;It could be under Drivers and Switches or Engine and DC motor control. All these are integrated circuits. &lt;/P&gt;&lt;P&gt;The Board tools available are these: &lt;A href="http://www.freescale.com/webapp/sps/site/overview.jsp?code=ANALOGTOOLBOX" title="http://www.freescale.com/webapp/sps/site/overview.jsp?code=ANALOGTOOLBOX"&gt;http://www.freescale.com/webapp/sps/site/overview.jsp?code=ANALOGTOOLBOX&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And just&amp;nbsp; to confirm, you have checked the following shield used for our Freescale Cup Challenges: &lt;A href="https://community.nxp.com/docs/DOC-1059"&gt;Freescale Cup Motor Driver Board. &lt;/A&gt; You can acquire it in our &lt;A href="https://community.nxp.com/www.freescale.com" target="test_blank"&gt;www.freescale.com&lt;/A&gt; with the part number TFC-Shield, it comes with the FRDM-KL25Z board.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Jan 2015 15:56:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/The-convinient-stepper-motor-driver-for-FRDM-KL25Z/m-p/376654#M19799</guid>
      <dc:creator>DamarisOchoa</dc:creator>
      <dc:date>2015-01-28T15:56:04Z</dc:date>
    </item>
    <item>
      <title>Re: The convinient stepper motor driver for FRDM-KL25Z</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/The-convinient-stepper-motor-driver-for-FRDM-KL25Z/m-p/376655#M19800</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/DamarisOchoa"&gt;DamarisOchoa&lt;/A&gt; maybe my question wasn't clear enough. I have a FRDM-KL25Z which av been trying to drive AT LEAST 4 Bipolar stepper motors. but i have not found the most convenient motor driver. I have a Pololu - DRV8825 Stepper Motor Driver Carrier which is causing me a lot of headache. It just doesnt work with the KL25Z. i also tested with L293D and ULN200XX which worked but required that i shift the voltage from 3v-5v in order 4 them 2 interface with the board. But now i want a dedicated stepper motor driver (with a carrier) which would interface directly with the board and work directly with the 3v logic from the board pins. I also need a driver board that doesnt sit on top of the KL25Z which will end up limiting the number of pins i use (e.g THE ARDUINO SHIELD &amp;gt;&amp;gt; &lt;A href="http://mcuoneclipse.com/2012/12/14/frdm-kl25z-with-the-arduino-motor-shield/" title="http://mcuoneclipse.com/2012/12/14/frdm-kl25z-with-the-arduino-motor-shield/"&gt;FRDM-KL25Z with the Arduino Motor Shield | MCU on Eclipse&lt;/A&gt;). therefore i need smth very small in size even if it drives 1 stepper motor i can be able to multiply them easily without my project becoming cumbersome. I hope that is clear enough.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Jan 2015 13:05:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/The-convinient-stepper-motor-driver-for-FRDM-KL25Z/m-p/376655#M19800</guid>
      <dc:creator>kevinamadiva</dc:creator>
      <dc:date>2015-01-29T13:05:52Z</dc:date>
    </item>
    <item>
      <title>Re: The convinient stepper motor driver for FRDM-KL25Z</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/The-convinient-stepper-motor-driver-for-FRDM-KL25Z/m-p/376656#M19801</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Kevin, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I checked who can help on this question and &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/vicentegomez"&gt;vicentegomez&lt;/A&gt; suggested to take this question to the &lt;A href="https://community.nxp.com/space/2019"&gt; Kinetis Microcontrollers&lt;/A&gt; Community where engineers can support with suggestions on Stepper Motor drivers. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards, &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Jan 2015 17:41:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/The-convinient-stepper-motor-driver-for-FRDM-KL25Z/m-p/376656#M19801</guid>
      <dc:creator>DamarisOchoa</dc:creator>
      <dc:date>2015-01-29T17:41:03Z</dc:date>
    </item>
    <item>
      <title>Re: The convinient stepper motor driver for FRDM-KL25Z</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/The-convinient-stepper-motor-driver-for-FRDM-KL25Z/m-p/376657#M19802</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can download the example driver that is used to control the &lt;A href="https://community.nxp.com/docs/DOC-93914"&gt;Freescale Cup Shield for the Freedom KL25Z&lt;/A&gt; which has on board 2 channel Motor Driver ICs (MC33887APVW). It might be helpful. Unfortunately we do not have a code driver for the bipolar stepper motors you are using.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this information can help you&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Adrian Sanchez Cano&lt;BR /&gt;Technical Support Engineer&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Feb 2015 17:05:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/The-convinient-stepper-motor-driver-for-FRDM-KL25Z/m-p/376657#M19802</guid>
      <dc:creator>adriancano</dc:creator>
      <dc:date>2015-02-03T17:05:04Z</dc:date>
    </item>
    <item>
      <title>Re: The convinient stepper motor driver for FRDM-KL25Z</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/The-convinient-stepper-motor-driver-for-FRDM-KL25Z/m-p/376658#M19803</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i just bought a few DRV8825 pololu driver chips and they work out of the box directly with the KL25Z. Worked like charm. So if it would be helpful for someone, i suggest using the DRV8825 driver chip. Thanks for the help though.... :-D&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Mar 2015 10:17:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/The-convinient-stepper-motor-driver-for-FRDM-KL25Z/m-p/376658#M19803</guid>
      <dc:creator>kevinamadiva</dc:creator>
      <dc:date>2015-03-16T10:17:08Z</dc:date>
    </item>
  </channel>
</rss>