<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: K53n512 Bricked</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K53n512-Bricked/m-p/376369#M19776</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Richard&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As long as you haven't set flash security to block erasing it may be simplest to use the EZ port to send a mass erase to the device. This requires just 3 signals to be connected and typical SPI Flash commands to be sent. There is an application note for an EZ port programmer on a KwikStik if you search the Freescale web site.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you have another Kinetis board you can also use this to do it by loading the uTasker project to it - it has an EZ port option which can be enabled which allows commands to be sent.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The uTasker project also includes support of the TWR-K53N512 (USB, Ethernet, SLCD etc.) (as well as most other KE, KL, and K parts out-of-the-box without needing to port from a few standard demo parts). It also allows you to simulate the Kinetis and the board in (approx.) real time so will improve development efficiency dramatically compared to traditional techniques.&lt;/P&gt;&lt;P&gt;Below is a screen shot of the project running the TWR-K53N512 and its SLCD. There is also a video of the SLCD in operation at &lt;A href="https://www.youtube.com/watch?v=nm2DmZv1rj8" title="https://www.youtube.com/watch?v=nm2DmZv1rj8"&gt;K40_SLCD.wmv - YouTube&lt;/A&gt; and some further details in &lt;A href="http://www.utasker.com/docs/uTasker/uTasker_SLCD.pdf" title="http://www.utasker.com/docs/uTasker/uTasker_SLCD.pdf"&gt;http://www.utasker.com/docs/uTasker/uTasker_SLCD.pdf&lt;/A&gt; (the video shows K40s in operation but the K53 is essentially equivalent for the SLCD interface)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/47707i6B488DAEAEF1C81A/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.utasker.com/kinetis.html" title="http://www.utasker.com/kinetis.html"&gt;http://www.utasker.com/kinetis.html&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 29 Nov 2014 00:58:10 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2014-11-29T00:58:10Z</dc:date>
    <item>
      <title>K53n512 Bricked</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K53n512-Bricked/m-p/376366#M19773</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;While minding my own business and innocently trying out 'example' programs:smileysilly:, I had 'processor expert' pop up in one of the IDE's I was&lt;/P&gt;&lt;P&gt;trying.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This has probably reconfigured internal GPIO assignments that control power/reset modes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;End of day, K53N512 tower board is bricked. The nice people at P + E Micro will gladly sell me (400 usd) a jlinkish debugger&lt;/P&gt;&lt;P&gt;and a mini app that prompts you to power up/down the board, and attempts to halt before the 'dangerous' area, and let you erase the flash.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hey Freescale - isn't there an easier way to erase the flash and start again non-brick mode?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Richie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Nov 2014 12:03:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K53n512-Bricked/m-p/376366#M19773</guid>
      <dc:creator>rcl-arm-coder</dc:creator>
      <dc:date>2014-11-27T12:03:17Z</dc:date>
    </item>
    <item>
      <title>Re: K53n512 Bricked</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K53n512-Bricked/m-p/376367#M19774</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it is possible that the reconfiguration of the GPIO affected the JTAG pins ans this is causing that behavior. You can try a mass erase how is showed in this post:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/376507"&gt;Re: PE multilink JTAG/BDM Kinetis programming issue&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also you can try to use the P&amp;amp;E Recovery Utility that is mentioned in this post by colleague Erich Styger:&lt;/P&gt;&lt;P&gt;&lt;A href="http://mcuoneclipse.com/2013/06/16/bricking-and-recovering-frdm-kl25z-boards-reset-swd-clock-and-low-power/" title="http://mcuoneclipse.com/2013/06/16/bricking-and-recovering-frdm-kl25z-boards-reset-swd-clock-and-low-power/"&gt;Bricking and Recovering FRDM-KL25Z Boards: Reset, SWD Clock and Low Power | MCU on Eclipse&lt;/A&gt;&lt;/P&gt;&lt;P&gt;For the TWR-K53 you need to select the USB Multilink (OSBDM) option and JTAG, please refer to the post for more information.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this information can help you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Adrian Sanchez Cano&lt;BR /&gt;Technical Support Engineer&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Nov 2014 19:31:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K53n512-Bricked/m-p/376367#M19774</guid>
      <dc:creator>adriancano</dc:creator>
      <dc:date>2014-11-28T19:31:55Z</dc:date>
    </item>
    <item>
      <title>Re: K53n512 Bricked</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K53n512-Bricked/m-p/376368#M19775</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Adrian&lt;/P&gt;&lt;P&gt;I read both of those recommended posts before posting the 'kn53 brick' post, because they do not answer the issue.&lt;/P&gt;&lt;P&gt;resources available to me:&lt;/P&gt;&lt;P&gt;1) KN53 tower kit (elevator boards, serial board, KN53 board)&amp;nbsp;- Every sw tool from PE Micro&amp;nbsp;- Kinetis Design Studio&amp;nbsp;- IAR (latest)&amp;nbsp;- Keil.microvision (latest)&amp;nbsp;- Last 5 current versions of Eclipse&amp;nbsp;- All SDK's, tools, examples from Freescale&amp;nbsp;- several varieties of J-Link debugger&lt;/P&gt;&lt;P&gt;&amp;nbsp;- Fully updates drivers for all of the above (sparing you the details)&lt;/P&gt;&lt;P&gt;In none of the above is a 'K53 example' for any of the IDE's, lots of K60 examples(especially in the K53 downloads!)&lt;/P&gt;&lt;P&gt;Assuming that development time is more important than the cost of another K53 tower board, and thatI 'start fresh' with a non-bricked board, what do you recommend as a development environment"ready to go" for the purpose of evaluating the K53 for our products ?&lt;/P&gt;&lt;P&gt;Cool features would be -&lt;/P&gt;&lt;HR originaltext="---" /&gt;&lt;P&gt;- real K53 'project' examples for the chosen (you suggest, I either already have it, or can get it) IDE&lt;/P&gt;&lt;P&gt;- low chance of making another brick, especially with Freescale's own tools and suggested configurations&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Don't stress too much about it, at the end of the day we will probably never build more than100,000 products with the K53 - it's not for consumer gear, so no real high volume.&lt;/P&gt;&lt;P&gt;It is however for products that will be used to protect people, prevent harm, look out for national security and hopefully make a difference. Visit kromek.com if curious.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;      From: Adrian Sanchez Cano &amp;lt;admin@community.freescale.com&amp;gt;&lt;/P&gt;&lt;P&gt; To: richard lowes &amp;lt;richardl10@rocketmail.com&amp;gt; &lt;/P&gt;&lt;P&gt; Sent: Friday, November 28, 2014 7:32 PM&lt;/P&gt;&lt;P&gt; Subject: Re:  - K53n512 Bricked&lt;/P&gt;&lt;P&gt;   &lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;|  &lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;| &lt;/P&gt;&lt;P&gt;K53n512 Bricked&lt;/P&gt;&lt;P&gt;reply from Adrian Sanchez Cano in  Kinetis Microcontrollers - View the full discussionHi,&amp;nbsp;it is possible that the reconfiguration of the GPIO affected the JTAG pins ans this is causing that behavior. You can try a mass erase how is showed in this post:Re: PE multilink JTAG/BDM Kinetis programming issue&amp;nbsp;Also you can try to use the P&amp;amp;E Recovery Utility that is mentioned in this post by colleague Erich Styger:Bricking and Recovering FRDM-KL25Z Boards: Reset, SWD Clock and Low Power | MCU on EclipseFor the TWR-K53 you need to select the USB Multilink (OSBDM) option and JTAG, please refer to the post for more information.&lt;/P&gt;&lt;P&gt;Hope this information can help you.&amp;nbsp;Best Regards,&lt;/P&gt;&lt;P&gt;Adrian Sanchez Cano&lt;/P&gt;&lt;P&gt;Technical Support Engineer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Nov 2014 23:28:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K53n512-Bricked/m-p/376368#M19775</guid>
      <dc:creator>rcl-arm-coder</dc:creator>
      <dc:date>2014-11-28T23:28:52Z</dc:date>
    </item>
    <item>
      <title>Re: K53n512 Bricked</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K53n512-Bricked/m-p/376369#M19776</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Richard&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As long as you haven't set flash security to block erasing it may be simplest to use the EZ port to send a mass erase to the device. This requires just 3 signals to be connected and typical SPI Flash commands to be sent. There is an application note for an EZ port programmer on a KwikStik if you search the Freescale web site.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you have another Kinetis board you can also use this to do it by loading the uTasker project to it - it has an EZ port option which can be enabled which allows commands to be sent.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The uTasker project also includes support of the TWR-K53N512 (USB, Ethernet, SLCD etc.) (as well as most other KE, KL, and K parts out-of-the-box without needing to port from a few standard demo parts). It also allows you to simulate the Kinetis and the board in (approx.) real time so will improve development efficiency dramatically compared to traditional techniques.&lt;/P&gt;&lt;P&gt;Below is a screen shot of the project running the TWR-K53N512 and its SLCD. There is also a video of the SLCD in operation at &lt;A href="https://www.youtube.com/watch?v=nm2DmZv1rj8" title="https://www.youtube.com/watch?v=nm2DmZv1rj8"&gt;K40_SLCD.wmv - YouTube&lt;/A&gt; and some further details in &lt;A href="http://www.utasker.com/docs/uTasker/uTasker_SLCD.pdf" title="http://www.utasker.com/docs/uTasker/uTasker_SLCD.pdf"&gt;http://www.utasker.com/docs/uTasker/uTasker_SLCD.pdf&lt;/A&gt; (the video shows K40s in operation but the K53 is essentially equivalent for the SLCD interface)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/47707i6B488DAEAEF1C81A/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.utasker.com/kinetis.html" title="http://www.utasker.com/kinetis.html"&gt;http://www.utasker.com/kinetis.html&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 29 Nov 2014 00:58:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K53n512-Bricked/m-p/376369#M19776</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2014-11-29T00:58:10Z</dc:date>
    </item>
  </channel>
</rss>