<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Kinetis Parametric Search missing full UART capability</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-Parametric-Search-missing-full-UART-capability/m-p/375995#M19742</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks - now it works. But yesterday it didn't - it was only showing 1,2,3,4 UARTs and also no family gave an indication of the max. available; many just showed a '.'.&lt;/P&gt;&lt;P&gt;Therefore there was either a problem recently or else someone has in fact done a good job to update the info within the last day!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 18 Sep 2014 10:31:29 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2014-09-18T10:31:29Z</dc:date>
    <item>
      <title>Kinetis Parametric Search missing full UART capability</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-Parametric-Search-missing-full-UART-capability/m-p/375993#M19740</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Freescale&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I gave a company advice about choosing a processor for a new project. One of the main criteria was that it should have at least 5 UARTs.&lt;/P&gt;&lt;P&gt;So I told them to check out the K-family and choose the type that best suited.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To my surprise I later heard that they abandonned this path since no Kinetis devices had more than 4 UARTs, which is of course incorrect because there are a number with 5 or 6 UARTs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For their research they used the Kinetis &lt;SPAN class="text"&gt;parametric search:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/parametricSelector.sp?&amp;amp;c=c201_c173&amp;amp;cof=0&amp;amp;am=0&amp;amp;sd=p727~N" title="http://www.freescale.com/webapp/parametricSelector.sp?&amp;amp;c=c201_c173&amp;amp;cof=0&amp;amp;am=0&amp;amp;sd=p727~N"&gt;http://www.freescale.com/webapp/parametricSelector.sp?&amp;amp;c=c201_c173&amp;amp;cof=0&amp;amp;am=0&amp;amp;sd=p727~N&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And indeed this only allows up to 4 UARTs to be selected as parameter and so they obviously gave up looking further.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is a bit of a shame because Freescale makes chips that would have been perfect for the job but trip up prospective customers at the start gate since they can't (simply) get the information that they need to make initial decisions as to whether they should look more deeply or not.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would at least add extra UARts to the search.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Sep 2014 13:33:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-Parametric-Search-missing-full-UART-capability/m-p/375993#M19740</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2014-09-17T13:33:44Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis Parametric Search missing full UART capability</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-Parametric-Search-missing-full-UART-capability/m-p/375994#M19741</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mark,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Actually I can search more than 4 UARTs with the link you provided, please kindly refer to the following for more details.&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/46037i20A9DF8D25FE7469/image-size/large?v=v2&amp;amp;px=999" title="1.png" alt="1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;is the above info that your customer looked for?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Sep 2014 08:26:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-Parametric-Search-missing-full-UART-capability/m-p/375994#M19741</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2014-09-18T08:26:05Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis Parametric Search missing full UART capability</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-Parametric-Search-missing-full-UART-capability/m-p/375995#M19742</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks - now it works. But yesterday it didn't - it was only showing 1,2,3,4 UARTs and also no family gave an indication of the max. available; many just showed a '.'.&lt;/P&gt;&lt;P&gt;Therefore there was either a problem recently or else someone has in fact done a good job to update the info within the last day!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Sep 2014 10:31:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-Parametric-Search-missing-full-UART-capability/m-p/375995#M19742</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2014-09-18T10:31:29Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis Parametric Search missing full UART capability</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-Parametric-Search-missing-full-UART-capability/m-p/375996#M19743</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mark,&lt;/P&gt;&lt;P&gt;Thanks for letting us know about this issue.&lt;/P&gt;&lt;P&gt;If you face another issue related to the "Product Selector" (was "Parametric Search"), please let me know posting a message on this group:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/groups/parametricfeedback"&gt;https://community.freescale.com/groups/parametricfeedback&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The goal of this group is to inform the new features, know issues and to hear all your feedback related to the tool. Also we are open to receive any information related to parameters needed for a better selection (e.g: Implement "EEPROM" on this product family).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mauricio.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Apr 2015 15:24:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-Parametric-Search-missing-full-UART-capability/m-p/375996#M19743</guid>
      <dc:creator>maugloria</dc:creator>
      <dc:date>2015-04-23T15:24:53Z</dc:date>
    </item>
  </channel>
</rss>