<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic K70 Pin mux with NAND flash in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-Pin-mux-with-NAND-flash/m-p/375899#M19731</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; I m routing the signals of K70 processor to NAND flash.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; In&amp;nbsp; K70 Processer the Pin PTC17 and PTC18 contains NFC_CE0 and NFC_CE1.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; In Tower kit the PTC17 is given to NAND flash .I would like to know that if i use PTC18 is given to NAND flash the signal function is same&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; between NFC_CE0 and NFC_CE1 or different?please assist me..............&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 26 Dec 2014 04:50:18 GMT</pubDate>
    <dc:creator>chiranjeevn</dc:creator>
    <dc:date>2014-12-26T04:50:18Z</dc:date>
    <item>
      <title>K70 Pin mux with NAND flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-Pin-mux-with-NAND-flash/m-p/375899#M19731</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; I m routing the signals of K70 processor to NAND flash.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; In&amp;nbsp; K70 Processer the Pin PTC17 and PTC18 contains NFC_CE0 and NFC_CE1.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; In Tower kit the PTC17 is given to NAND flash .I would like to know that if i use PTC18 is given to NAND flash the signal function is same&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; between NFC_CE0 and NFC_CE1 or different?please assist me..............&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Dec 2014 04:50:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-Pin-mux-with-NAND-flash/m-p/375899#M19731</guid>
      <dc:creator>chiranjeevn</dc:creator>
      <dc:date>2014-12-26T04:50:18Z</dc:date>
    </item>
    <item>
      <title>Re: K70 Pin mux with NAND flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-Pin-mux-with-NAND-flash/m-p/375900#M19732</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NFC_CE is the signal to enable Flash chip.&lt;/P&gt;&lt;P&gt;NFC_CE0 and NFC_CE1 is in fact used as the flash chip select pin.&lt;/P&gt;&lt;P&gt;the signals on both pins are same, you can certainly connect PTC17 or PTC18 to your flash chip if there is only one NAND flash on the board.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Dec 2014 06:04:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K70-Pin-mux-with-NAND-flash/m-p/375900#M19732</guid>
      <dc:creator>Rick_Li</dc:creator>
      <dc:date>2014-12-26T06:04:27Z</dc:date>
    </item>
  </channel>
</rss>