<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Kinetis register for analog voltage like S12</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-register-for-analog-voltage-like-S12/m-p/375638#M19711</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Scott,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If customer want to config Kinetis analog pin as GPIO input function, and check the GPIO input data register to check the voltage level(high or low)?&lt;/P&gt;&lt;P&gt;If so, yes, Kinetis product with this function.&lt;/P&gt;&lt;P&gt;Customer can set most analog pin as GPIO input function using Pin Control Register n (PORTx_PCRn) [MUX] bits select related pin function.&lt;/P&gt;&lt;P&gt;And the Port Data Input Register (GPIOx_PDIR) register will reflect the input voltage level.&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;best regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 15 Feb 2015 02:15:48 GMT</pubDate>
    <dc:creator>Hui_Ma</dc:creator>
    <dc:date>2015-02-15T02:15:48Z</dc:date>
    <item>
      <title>Kinetis register for analog voltage like S12</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-register-for-analog-voltage-like-S12/m-p/375637#M19710</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;Hello,&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;Do the Kinetis parts have a register that indicates the digital state of the voltage on any analog pin?&amp;nbsp; The S12 had a feature like this.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;Thanks.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;Scott&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Feb 2015 18:15:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-register-for-analog-voltage-like-S12/m-p/375637#M19710</guid>
      <dc:creator>ScottKerstein</dc:creator>
      <dc:date>2015-02-13T18:15:15Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis register for analog voltage like S12</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-register-for-analog-voltage-like-S12/m-p/375638#M19711</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Scott,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If customer want to config Kinetis analog pin as GPIO input function, and check the GPIO input data register to check the voltage level(high or low)?&lt;/P&gt;&lt;P&gt;If so, yes, Kinetis product with this function.&lt;/P&gt;&lt;P&gt;Customer can set most analog pin as GPIO input function using Pin Control Register n (PORTx_PCRn) [MUX] bits select related pin function.&lt;/P&gt;&lt;P&gt;And the Port Data Input Register (GPIOx_PDIR) register will reflect the input voltage level.&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;best regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 15 Feb 2015 02:15:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-register-for-analog-voltage-like-S12/m-p/375638#M19711</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2015-02-15T02:15:48Z</dc:date>
    </item>
  </channel>
</rss>