<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: EEPROM TWRkit</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/EEPROM-TWRkit/m-p/375555#M19706</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I just notice that I get the TWR_K60N512 and there is not FLEXNVM memory, it is a devices with program flash only.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So I can use the flash to store all the data? How can I setup the flash part (at that range adress 0x1400_0000–0x17FF_FFFF) to b able to use it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any example?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 22 Aug 2014 19:34:52 GMT</pubDate>
    <dc:creator>xavierbuhot</dc:creator>
    <dc:date>2014-08-22T19:34:52Z</dc:date>
    <item>
      <title>EEPROM TWRkit</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/EEPROM-TWRkit/m-p/375554#M19705</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I would like to use the eeprom on my k60 kinetis so I found the example supply with th TWRkit.&lt;/P&gt;&lt;P&gt;When I launch the program the EEPROM still lock and never ready, the program are still running at that sentence:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;/* Wait for the command to complete */&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;while(!(FTFL_FCNFG &amp;amp; FTFL_FCNFG_EEERDY_MASK));&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can someone help me?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regard.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Aug 2014 09:49:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/EEPROM-TWRkit/m-p/375554#M19705</guid>
      <dc:creator>xavierbuhot</dc:creator>
      <dc:date>2014-08-22T09:49:38Z</dc:date>
    </item>
    <item>
      <title>Re: EEPROM TWRkit</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/EEPROM-TWRkit/m-p/375555#M19706</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I just notice that I get the TWR_K60N512 and there is not FLEXNVM memory, it is a devices with program flash only.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So I can use the flash to store all the data? How can I setup the flash part (at that range adress 0x1400_0000–0x17FF_FFFF) to b able to use it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any example?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Aug 2014 19:34:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/EEPROM-TWRkit/m-p/375555#M19706</guid>
      <dc:creator>xavierbuhot</dc:creator>
      <dc:date>2014-08-22T19:34:52Z</dc:date>
    </item>
    <item>
      <title>Re: EEPROM TWRkit</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/EEPROM-TWRkit/m-p/375556#M19707</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;More informations about my problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I try to put my program into RAM and try to write on flash blocks. But I still have Hard fault and vector 3 interrupt.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it really possible to write in flash memory?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please ... :smileysad:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Aug 2014 19:16:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/EEPROM-TWRkit/m-p/375556#M19707</guid>
      <dc:creator>xavierbuhot</dc:creator>
      <dc:date>2014-08-25T19:16:37Z</dc:date>
    </item>
    <item>
      <title>Re: EEPROM TWRkit</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/EEPROM-TWRkit/m-p/375557#M19708</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Xavier:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I noticed you submitted a Service Request about these questions. Are your doubts clarified?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Just to summarize:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- You are correct, K60N512 does not have Flex NVM. But yes, you can still use part of the program flash to store non volatile data.&lt;/P&gt;&lt;P&gt;- You cannot use range 0x1400_0000–0x17FF_FFFF, since this is not present in your&amp;nbsp; device.&lt;/P&gt;&lt;P&gt;- The available flash memory in K60N512 is from 0x00000000 to 0x0007FFFF.&lt;/P&gt;&lt;P&gt;- For Flash memory storage and code examples, you can refer to Freescale Standard Software Driver (C90TFS), downloadable from the next link:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/32bit/software/C90TFS_FLASH_DRIVER.exe" title="http://cache.freescale.com/files/32bit/software/C90TFS_FLASH_DRIVER.exe"&gt;http://cache.freescale.com/files/32bit/software/C90TFS_FLASH_DRIVER.exe&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Sep 2014 02:01:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/EEPROM-TWRkit/m-p/375557#M19708</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2014-09-09T02:01:57Z</dc:date>
    </item>
    <item>
      <title>Re: EEPROM TWRkit</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/EEPROM-TWRkit/m-p/375558#M19709</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your attention.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I finally achieve to ake it work. In my message I made a mistake, I did&lt;/P&gt;&lt;P&gt;wrote in the right part of the memory (0x00000000 to 0x0007FFFF.) but I&lt;/P&gt;&lt;P&gt;forget to setup the configuration of the flash memory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you again.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regard.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2014-09-09 4:02 GMT+02:00 Jorge_Gonzalez &amp;lt;admin@community.freescale.com&amp;gt;:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE level="1"&gt;&lt;P&gt;       &amp;lt;https://community.freescale.com/&amp;gt;&lt;/P&gt;&lt;P&gt;EEPROM TWRkit&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;reply from Jorge_Gonzalez&lt;/P&gt;&lt;P&gt;&amp;lt;https://community.freescale.com/people/Jorge_Gonzalez?et=watches.email.thread&amp;gt;&lt;/P&gt;&lt;P&gt;in * Kinetis Microcontrollers* - View the full discussion&lt;/P&gt;&lt;P&gt;&amp;lt;https://community.freescale.com/message/433553?et=watches.email.thread#433553&amp;gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Sep 2014 18:00:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/EEPROM-TWRkit/m-p/375558#M19709</guid>
      <dc:creator>xavierbuhot</dc:creator>
      <dc:date>2014-09-09T18:00:53Z</dc:date>
    </item>
  </channel>
</rss>