<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Is the KE02 SWD_DIO, SWD_CLK require external pullup/down resistors?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-the-KE02-SWD-DIO-SWD-CLK-require-external-pullup-down/m-p/373786#M19525</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Isao:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry for the time with no responses. Regarding your questions:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;1)&lt;/STRONG&gt; The recommended range is from 4.7KΩ to 10KΩ.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;2)&lt;/STRONG&gt; Pulldown resistor is used for signal stability purposes. There are no restrictions but you may not be able to program the MCU.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;3)&lt;/STRONG&gt; SWD_DIO pin has an internal pullup, so external pullup is recommended but not necessary.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 24 Sep 2014 17:02:25 GMT</pubDate>
    <dc:creator>Jorge_Gonzalez</dc:creator>
    <dc:date>2014-09-24T17:02:25Z</dc:date>
    <item>
      <title>Is the KE02 SWD_DIO, SWD_CLK require external pullup/down resistors?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-the-KE02-SWD-DIO-SWD-CLK-require-external-pullup-down/m-p/373785#M19524</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;According to the note 1 in 9.2 Debug port pin descriptions of KE02 reference manual, we need to add external pulldown resistor for the SWD_CLK to fully support SWD protocol.&lt;/P&gt;&lt;P&gt;Please advise the below questions as soon as possible.&lt;/P&gt;&lt;P&gt;1. Please tell us recommended pulldown resistor value.&lt;/P&gt;&lt;P&gt;2. Please tell us restriction if we don't add external pulldown resistor.&lt;/P&gt;&lt;P&gt;3. Is the SWD_DIO require pullup or pulldown resistor to fully support SWD protocol?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Takashima&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Sep 2014 06:24:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-the-KE02-SWD-DIO-SWD-CLK-require-external-pullup-down/m-p/373785#M19524</guid>
      <dc:creator>isaotakashima</dc:creator>
      <dc:date>2014-09-17T06:24:08Z</dc:date>
    </item>
    <item>
      <title>Re: Is the KE02 SWD_DIO, SWD_CLK require external pullup/down resistors?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-the-KE02-SWD-DIO-SWD-CLK-require-external-pullup-down/m-p/373786#M19525</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Isao:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry for the time with no responses. Regarding your questions:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;1)&lt;/STRONG&gt; The recommended range is from 4.7KΩ to 10KΩ.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;2)&lt;/STRONG&gt; Pulldown resistor is used for signal stability purposes. There are no restrictions but you may not be able to program the MCU.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;3)&lt;/STRONG&gt; SWD_DIO pin has an internal pullup, so external pullup is recommended but not necessary.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Sep 2014 17:02:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Is-the-KE02-SWD-DIO-SWD-CLK-require-external-pullup-down/m-p/373786#M19525</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2014-09-24T17:02:25Z</dc:date>
    </item>
  </channel>
</rss>