<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: __thumb_startup(void) function issue</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/thumb-startup-void-function-issue/m-p/372631#M19420</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Li,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, of course but how do I upload it here? There is no attachment option in here.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 25 Dec 2014 23:39:25 GMT</pubDate>
    <dc:creator>manuchehrebrahi</dc:creator>
    <dc:date>2014-12-25T23:39:25Z</dc:date>
    <item>
      <title>__thumb_startup(void) function issue</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/thumb-startup-void-function-issue/m-p/372626#M19415</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is no interrupt used on the test code that I have as well as I didn't add COP (Watchdog Timer) to the components. However on the debug mode, when it runs in Resume mode, it calls __thumb_startup(void) function which I believe it CPU reset function handler, but when it goes to step by step then, it never call that function and stays in the main routine. Please let me know if you have any comment on this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Dec 2014 23:03:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/thumb-startup-void-function-issue/m-p/372626#M19415</guid>
      <dc:creator>manuchehrebrahi</dc:creator>
      <dc:date>2014-12-23T23:03:51Z</dc:date>
    </item>
    <item>
      <title>Re: __thumb_startup(void) function issue</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/thumb-startup-void-function-issue/m-p/372627#M19416</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Space,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It looks lice the device made a reset, there can be many reasons for this, &lt;/P&gt;&lt;P&gt;like stack overflow , accessing illegal instructions ....&lt;/P&gt;&lt;P&gt;And&amp;nbsp; there is another possible , please check your code , whether had a breakpoint&amp;nbsp; on the function which is not linked or not used now .&lt;/P&gt;&lt;P&gt;&lt;A href="http://mcuoneclipse.com/2014/10/11/failed-to-debug-with-gdb-breakpoints-or-expressions-on-non-existing-locations/" title="http://mcuoneclipse.com/2014/10/11/failed-to-debug-with-gdb-breakpoints-or-expressions-on-non-existing-locations/"&gt;" Failed to Debug with GDB: Breakpoints or Expressions on non-existing Locations | MCU on Eclipse&lt;/A&gt; "&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Dec 2014 02:03:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/thumb-startup-void-function-issue/m-p/372627#M19416</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2014-12-24T02:03:21Z</dc:date>
    </item>
    <item>
      <title>Re: __thumb_startup(void) function issue</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/thumb-startup-void-function-issue/m-p/372628#M19417</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alice and thanks for your reply. We just running out of project time and I was thinking we may have to switch to other MCU. It is really good to hear someone is there.&lt;/P&gt;&lt;P&gt;On the debug, I see check marked breakpoints on the main function which is not generated by me. This is the message after the flashing program to the board, on the console it says,&lt;/P&gt;&lt;P&gt;------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;The target endianness is set automatically (currently little endian)&lt;/P&gt;&lt;P&gt;continue&lt;/P&gt;&lt;P&gt;Continuing.&lt;/P&gt;&lt;P&gt;Note: automatically using hardware breakpoints for read-only addresses.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Temporary breakpoint 1, main () at ../Sources/main.c:58&lt;/P&gt;&lt;P&gt;58&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PE_low_level_init();&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //End of Processor Expert internal initialization.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Quit (expect signal SIGINT when the program is resumed)&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;I have no idea why it generates Temporary breakpoint 1.&lt;/P&gt;&lt;P&gt;First I thought it might be watchdog timer but loop is so small as you can see on the code below and beside I haven't added watchdog timer yet. Looking forward to have your comments.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; pos.x = 0;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; pos.y = 0;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; pos.page = 0;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; DVS_CS1_ClrVal(NULL);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Unselect CS1&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; DVS_CS2_SetVal(NULL);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Select CS2&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; DVS_WriteByte(DVS_ON, DVS_Ins);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Power on&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; for (uint8_t i=0; i&amp;lt;8; i++)&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; *******&lt;SPAN style="text-decoration: underline;"&gt;&lt;EM&gt;&lt;STRONG&gt;This is where main program calls __thumb_startuo(void) function only if it runs continuously but trying step by step, (F5) it works fine and comes out of the "for" loop.&lt;/STRONG&gt;&lt;/EM&gt;&lt;/SPAN&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; DVS_Fill(CLEAR,0,2,i);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Clear Display, Dec23 127-&amp;gt; 2 for test&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; DVS_GotoXY(0,0);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;void DVS_Fill(uint8_t mode, uint8_t x1, uint8_t x2, uint8_t Row)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint8_t pi;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; for(pi=x1; pi&amp;lt;x2+1; pi++)&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;STRONG&gt;&lt;EM style="text-decoration: underline;"&gt;*******Same as above if you pass that loop with F5 it will call&lt;/EM&gt;&lt;/STRONG&gt; &lt;SPAN style="text-decoration: underline;"&gt;&lt;EM&gt;&lt;STRONG&gt;__thumb_startuo(void) function here. That only if it runs continuously but trying step by step, (F5) it works fine and comes out of the "for" loop.&lt;/STRONG&gt;&lt;/EM&gt;&lt;/SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; DVS_GotoXP(pi, Row);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; DVS_WriteByte(mode, DVS_Data);&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Dec 2014 14:57:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/thumb-startup-void-function-issue/m-p/372628#M19417</guid>
      <dc:creator>manuchehrebrahi</dc:creator>
      <dc:date>2014-12-24T14:57:36Z</dc:date>
    </item>
    <item>
      <title>Re: __thumb_startup(void) function issue</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/thumb-startup-void-function-issue/m-p/372629#M19418</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I made code so small (just one function to call) and compiled the program. It compiled it with no error like before. Then tried to flash the program to the MCU on the FRDM but then shows this message in Red,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;No source available for "(gdb[12].proc[42000].threadGroup[i1],gdb[12].proc[42000].OSthread[1]).thread[1].frame[0]" &lt;/P&gt;&lt;P&gt;View Disassembly &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I looked at Disassembly, I saw that it calls the &lt;SPAN style="text-decoration: underline;"&gt;&lt;EM&gt;&lt;STRONG&gt;__thumb_startuo(void) function.&lt;/STRONG&gt;&lt;/EM&gt;&lt;/SPAN&gt; So now question is what is causing these message after trying to program MCU on the FRDM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Dec 2014 15:32:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/thumb-startup-void-function-issue/m-p/372629#M19418</guid>
      <dc:creator>manuchehrebrahi</dc:creator>
      <dc:date>2014-12-24T15:32:20Z</dc:date>
    </item>
    <item>
      <title>Re: __thumb_startup(void) function issue</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/thumb-startup-void-function-issue/m-p/372630#M19419</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Can you please upload your new created program here for further investigating?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Dec 2014 06:23:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/thumb-startup-void-function-issue/m-p/372630#M19419</guid>
      <dc:creator>Rick_Li</dc:creator>
      <dc:date>2014-12-25T06:23:31Z</dc:date>
    </item>
    <item>
      <title>Re: __thumb_startup(void) function issue</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/thumb-startup-void-function-issue/m-p/372631#M19420</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Li,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, of course but how do I upload it here? There is no attachment option in here.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Dec 2014 23:39:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/thumb-startup-void-function-issue/m-p/372631#M19420</guid>
      <dc:creator>manuchehrebrahi</dc:creator>
      <dc:date>2014-12-25T23:39:25Z</dc:date>
    </item>
    <item>
      <title>Re: __thumb_startup(void) function issue</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/thumb-startup-void-function-issue/m-p/372632#M19421</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp; Space,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When you want upload attchment,&amp;nbsp; please click here :&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/48791i1B036C070F0C650E/image-size/large?v=v2&amp;amp;px=999" role="button" title="1.png" alt="1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;then &lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/48792iE9022AD3F8471C1B/image-size/large?v=v2&amp;amp;px=999" role="button" title="2.png" alt="2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Dec 2014 08:45:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/thumb-startup-void-function-issue/m-p/372632#M19421</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2014-12-26T08:45:08Z</dc:date>
    </item>
    <item>
      <title>Re: __thumb_startup(void) function issue</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/thumb-startup-void-function-issue/m-p/372633#M19422</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alice and Happy New Year!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am sure you are busy with lots of things came up over the holiday but I was wondering if you have received the files that I uploaded and had a chance to look at that. I look forward to hear from you on this matter.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Jan 2015 17:23:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/thumb-startup-void-function-issue/m-p/372633#M19422</guid>
      <dc:creator>manuchehrebrahi</dc:creator>
      <dc:date>2015-01-07T17:23:59Z</dc:date>
    </item>
    <item>
      <title>Re: __thumb_startup(void) function issue</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/thumb-startup-void-function-issue/m-p/372634#M19423</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Space4,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Happy New Year to you !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have received anything . ON the web , there has not your reply before you this reply.&lt;/P&gt;&lt;P&gt;Could you send it again .I will check as soon as possilbe.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Jan 2015 10:30:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/thumb-startup-void-function-issue/m-p/372634#M19423</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2015-01-08T10:30:00Z</dc:date>
    </item>
  </channel>
</rss>