<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: USB min frequency</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-min-frequency/m-p/372163#M19383</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/45981i9D36892AFD167623/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I run the uTasker USB-HID mouse on the FRDM-KL26Z I can set the system clock to 24MHz and the Flash/Bus clocks to 3MHz and build with GCC with no optimisation and it operates normally (connected &amp;gt;20 times without any errors). Generally there shouldn't be much time critical with the enumeration process.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 17 Sep 2014 00:24:09 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2014-09-17T00:24:09Z</dc:date>
    <item>
      <title>USB min frequency</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-min-frequency/m-p/372162#M19382</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;what's the min CPU frequency Freesscale bare metal USB stack (namely generic HID device) can reliably run on KL26?&lt;/P&gt;&lt;P&gt;I clock USB module 48 MHz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I compile my C code without optimization and CPU runs on 12 MHz I mainly get "USB device not recognized" error in Windows when I connect my device to PC (90% probability I will get the error)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;No optimization and 24 Mhz CPU leads to "USB device cannot start, Code 10" in Windows (10 % probabality I will get the error)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Optimization and 12 MHz CPU leads to "USB device cannot start, Code 10" in Windows (10 % probabality I will get the error)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Optimization and 24 Mhz leads to no error.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Sep 2014 14:56:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-min-frequency/m-p/372162#M19382</guid>
      <dc:creator>martindusek</dc:creator>
      <dc:date>2014-09-16T14:56:42Z</dc:date>
    </item>
    <item>
      <title>Re: USB min frequency</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-min-frequency/m-p/372163#M19383</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/45981i9D36892AFD167623/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I run the uTasker USB-HID mouse on the FRDM-KL26Z I can set the system clock to 24MHz and the Flash/Bus clocks to 3MHz and build with GCC with no optimisation and it operates normally (connected &amp;gt;20 times without any errors). Generally there shouldn't be much time critical with the enumeration process.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Sep 2014 00:24:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/USB-min-frequency/m-p/372163#M19383</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2014-09-17T00:24:09Z</dc:date>
    </item>
  </channel>
</rss>