<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 FlexRAM as EEPROM</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexRAM-as-EEPROM/m-p/371915#M19350</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class="j-post-author"&gt;&lt;SPAN class="font-color-meta-light j-thread-replyto"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to have more help on the subject of FlexRAM as EEPROM. I am using a K20DX256 and Kinetis Design Studio (KDS) and I would like to use the FlexRAM + FlexNVM + EEEController to store some data with endurance as a normal EEPROM would be.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From AN4282 : Using the Kinetis Family Enhanced EEPROM Functionality :&lt;/P&gt;&lt;P&gt;“How FlexMemory EEE works&lt;/P&gt;&lt;P&gt;To provide enhanced EEPROM functionality, the FlexMemory uses a RAM block (FlexRAM), a flash&lt;/P&gt;&lt;P&gt;block (FlexNVM), and EEE state machine. When the EEE functionality is enabled, the FlexRAM becomes&lt;/P&gt;&lt;P&gt;your EEE memory. The FlexRAM address space is where you access all of your EEE data. When the EEE&lt;/P&gt;&lt;P&gt;is accessed, the EEE state machine keeps track of the data and backs it up as data records, stored in some&lt;/P&gt;&lt;P&gt;portion of the FlexNVM used as an E-flash. Using a large block of E-flash to back up the data for a smaller&lt;/P&gt;&lt;P&gt;amount of EEE data allows the FlexMemory EEE implementation to offer extremely high endurance.&lt;/P&gt;&lt;P&gt;”&lt;/P&gt;&lt;P&gt;My guess is I need to access the FlexRAM to access the FlexNVM and from the Reference Manual,&amp;nbsp; FlexRAM address range = 0x1400_0000 – 0x1400_07FF.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think I have all the bits configured right in the CPU component of Processor Expert regarding the Flex Memory Settings and the configuration of the ROM/RAM areas in the Build Options tab too.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My trouble resides in the way of writting and reading the data in the FlexRAM, anyone has a clue on how to proceed? And if there are PExp componants already made for this purpose?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;MH&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(I have already consulted and posted here: &lt;A _jive_internal="true" href="https://community.nxp.com/thread/328422"&gt;https://community.freescale.com/thread/328422&lt;/A&gt;)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 Feb 2015 18:43:32 GMT</pubDate>
    <dc:creator>mevon</dc:creator>
    <dc:date>2015-02-12T18:43:32Z</dc:date>
    <item>
      <title>FlexRAM as EEPROM</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexRAM-as-EEPROM/m-p/371915#M19350</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN class="j-post-author"&gt;&lt;SPAN class="font-color-meta-light j-thread-replyto"&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to have more help on the subject of FlexRAM as EEPROM. I am using a K20DX256 and Kinetis Design Studio (KDS) and I would like to use the FlexRAM + FlexNVM + EEEController to store some data with endurance as a normal EEPROM would be.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From AN4282 : Using the Kinetis Family Enhanced EEPROM Functionality :&lt;/P&gt;&lt;P&gt;“How FlexMemory EEE works&lt;/P&gt;&lt;P&gt;To provide enhanced EEPROM functionality, the FlexMemory uses a RAM block (FlexRAM), a flash&lt;/P&gt;&lt;P&gt;block (FlexNVM), and EEE state machine. When the EEE functionality is enabled, the FlexRAM becomes&lt;/P&gt;&lt;P&gt;your EEE memory. The FlexRAM address space is where you access all of your EEE data. When the EEE&lt;/P&gt;&lt;P&gt;is accessed, the EEE state machine keeps track of the data and backs it up as data records, stored in some&lt;/P&gt;&lt;P&gt;portion of the FlexNVM used as an E-flash. Using a large block of E-flash to back up the data for a smaller&lt;/P&gt;&lt;P&gt;amount of EEE data allows the FlexMemory EEE implementation to offer extremely high endurance.&lt;/P&gt;&lt;P&gt;”&lt;/P&gt;&lt;P&gt;My guess is I need to access the FlexRAM to access the FlexNVM and from the Reference Manual,&amp;nbsp; FlexRAM address range = 0x1400_0000 – 0x1400_07FF.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think I have all the bits configured right in the CPU component of Processor Expert regarding the Flex Memory Settings and the configuration of the ROM/RAM areas in the Build Options tab too.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My trouble resides in the way of writting and reading the data in the FlexRAM, anyone has a clue on how to proceed? And if there are PExp componants already made for this purpose?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;MH&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(I have already consulted and posted here: &lt;A _jive_internal="true" href="https://community.nxp.com/thread/328422"&gt;https://community.freescale.com/thread/328422&lt;/A&gt;)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Feb 2015 18:43:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexRAM-as-EEPROM/m-p/371915#M19350</guid>
      <dc:creator>mevon</dc:creator>
      <dc:date>2015-02-12T18:43:32Z</dc:date>
    </item>
    <item>
      <title>Re: FlexRAM as EEPROM</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexRAM-as-EEPROM/m-p/371916#M19351</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please, send your post to kinetis community (e.g. Kinetis Microcontrollers ) to get it visible for active members.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Soledad&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Feb 2015 18:46:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexRAM-as-EEPROM/m-p/371916#M19351</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2015-02-12T18:46:37Z</dc:date>
    </item>
    <item>
      <title>Re: FlexRAM as EEPROM</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexRAM-as-EEPROM/m-p/371917#M19352</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you very much! I was wondering about that, I guess I'm lucky you helped me!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Feb 2015 21:18:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexRAM-as-EEPROM/m-p/371917#M19352</guid>
      <dc:creator>mevon</dc:creator>
      <dc:date>2015-02-12T21:18:58Z</dc:date>
    </item>
  </channel>
</rss>