<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Problem with ADC on 64k version of KL14 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-with-ADC-on-64k-version-of-KL14/m-p/371884#M19348</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a project using KDS that uses the 32k version of the KL14 to read 8 ADC lines. This works perfectly, no issues at all. I had to increase the flash on a different project, so I decided to move both of them to the 64k version. Using PE, I added the 64k processor and set it all up. The problem, is that when I program the 64k chip, the ADCs all return 0. If I go back to the 32k chip, everything reads correctly. I am completely baffled. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I even set up a completely new project using the KL14Z64VTF4, and just added the ADCs to the project, and they all read 0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyone have any ideas? I can obviously go back to the 32k chip for this project, but this is driving me nuts.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 Feb 2015 19:11:25 GMT</pubDate>
    <dc:creator>Bretta</dc:creator>
    <dc:date>2015-02-12T19:11:25Z</dc:date>
    <item>
      <title>Problem with ADC on 64k version of KL14</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-with-ADC-on-64k-version-of-KL14/m-p/371884#M19348</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a project using KDS that uses the 32k version of the KL14 to read 8 ADC lines. This works perfectly, no issues at all. I had to increase the flash on a different project, so I decided to move both of them to the 64k version. Using PE, I added the 64k processor and set it all up. The problem, is that when I program the 64k chip, the ADCs all return 0. If I go back to the 32k chip, everything reads correctly. I am completely baffled. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I even set up a completely new project using the KL14Z64VTF4, and just added the ADCs to the project, and they all read 0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyone have any ideas? I can obviously go back to the 32k chip for this project, but this is driving me nuts.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Feb 2015 19:11:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-with-ADC-on-64k-version-of-KL14/m-p/371884#M19348</guid>
      <dc:creator>Bretta</dc:creator>
      <dc:date>2015-02-12T19:11:25Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with ADC on 64k version of KL14</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-with-ADC-on-64k-version-of-KL14/m-p/371885#M19349</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;Please, send your post to kinetis community (e.g. Kinetis Microcontrollers ) to get it visible for active members.&amp;nbsp; &lt;/P&gt;&lt;P&gt;Regards&amp;nbsp; &lt;/P&gt;&lt;P&gt;Soledad&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Feb 2015 20:36:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-with-ADC-on-64k-version-of-KL14/m-p/371885#M19349</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2015-02-12T20:36:03Z</dc:date>
    </item>
  </channel>
</rss>