<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: FRDM-Kx boards not in processor expert in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-Kx-boards-not-in-processor-expert/m-p/371146#M19284</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Kevin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The only support for boards that Processor Expert adds is that it creates some components already configured for the boards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For example, for the FRDM-KL25 there is a Red_LED component, that is basically a GPIO component with a custom name and the pin already configured to the one that is connected to the red pin of the RGB Led in the board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But all the microcontrollers used in the boards you mention are already supported in Processor Expert, so you can begin to work with all the boards immediately.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Santiago&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 06 Oct 2014 17:41:30 GMT</pubDate>
    <dc:creator>santiago_gonzal</dc:creator>
    <dc:date>2014-10-06T17:41:30Z</dc:date>
    <item>
      <title>FRDM-Kx boards not in processor expert</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-Kx-boards-not-in-processor-expert/m-p/371145#M19283</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;While having to go back to the drawing board for a 'lower' cost solution I looked at the KE0x and KL0x lines, I found support for the processors in Process Expert but the 'Board' support was not there:&lt;/P&gt;&lt;P&gt;FRDM-KE02Z40M&lt;/P&gt;&lt;P&gt;FRDM-KE02Z&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;FRDM-KL02Z&lt;/P&gt;&lt;P&gt;FRDM-KL03Z&lt;/P&gt;&lt;P&gt;FDRM-KL46Z&lt;/P&gt;&lt;P&gt;FRDM-K64F&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have the KL46Z and K64F but those are not supported in PE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any idea when the FRDM boards will be supported in PE? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MKL02Z16VFK4 is high on my list as well as the MKL03Z16VFG4. &lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Oct 2014 17:31:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-Kx-boards-not-in-processor-expert/m-p/371145#M19283</guid>
      <dc:creator>kevinangus</dc:creator>
      <dc:date>2014-10-06T17:31:10Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-Kx boards not in processor expert</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-Kx-boards-not-in-processor-expert/m-p/371146#M19284</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Kevin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The only support for boards that Processor Expert adds is that it creates some components already configured for the boards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For example, for the FRDM-KL25 there is a Red_LED component, that is basically a GPIO component with a custom name and the pin already configured to the one that is connected to the red pin of the RGB Led in the board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But all the microcontrollers used in the boards you mention are already supported in Processor Expert, so you can begin to work with all the boards immediately.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Santiago&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Oct 2014 17:41:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-Kx-boards-not-in-processor-expert/m-p/371146#M19284</guid>
      <dc:creator>santiago_gonzal</dc:creator>
      <dc:date>2014-10-06T17:41:30Z</dc:date>
    </item>
  </channel>
</rss>