<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: MD20DX128VFM5: USB ID Pin</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MD20DX128VFM5-USB-ID-Pin/m-p/371096#M19282</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Hui Shao:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That register usually causes confusion, sorry about that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In Kinetis MCUs the USBx_OTGSTAT register is not used and there is not a dedicated USB_ID pin, so you will not find it in the pinout table.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To handle the ID pin in the physical USB connectors, you can use any digital GPIO pin configured for interrupt.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the Freescale Tower System (e.g. TWR-SER) you can see that an external OTG Driver IC (MAX3353) is used. With this chip you can monitor the ID signal in two ways:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;1-&lt;/STRONG&gt; Using the ID_OUT pin of external driver IC.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;2-&lt;/STRONG&gt; Reading the ID status via the I2C communication with the driver IC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Some reference boards as &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=TWR-K20D50M&amp;amp;tid=m32TWR"&gt;&lt;STRONG&gt;TWR-K20D50M&lt;/STRONG&gt;&lt;/A&gt; already have the USB_ID pin connected to a GPIO so that it can be monitored by the application.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For more details on this check the next thread:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/311766"&gt;K60 USB FS/LS OTG Controller: Few questions&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps with your doubt.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 07 Oct 2014 02:15:24 GMT</pubDate>
    <dc:creator>Jorge_Gonzalez</dc:creator>
    <dc:date>2014-10-07T02:15:24Z</dc:date>
    <item>
      <title>MD20DX128VFM5: USB ID Pin</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MD20DX128VFM5-USB-ID-Pin/m-p/371095#M19281</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi -&lt;/P&gt;&lt;P&gt;Anyone knows where the USB ID pin described below is mapped to which physical pin on MK20DX128VFM5? I don't see it to pin configuration table.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/46407i510647276A32CAB4/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hui&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Oct 2014 17:24:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MD20DX128VFM5-USB-ID-Pin/m-p/371095#M19281</guid>
      <dc:creator>huishao2</dc:creator>
      <dc:date>2014-10-06T17:24:25Z</dc:date>
    </item>
    <item>
      <title>Re: MD20DX128VFM5: USB ID Pin</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MD20DX128VFM5-USB-ID-Pin/m-p/371096#M19282</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Hui Shao:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That register usually causes confusion, sorry about that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In Kinetis MCUs the USBx_OTGSTAT register is not used and there is not a dedicated USB_ID pin, so you will not find it in the pinout table.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To handle the ID pin in the physical USB connectors, you can use any digital GPIO pin configured for interrupt.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the Freescale Tower System (e.g. TWR-SER) you can see that an external OTG Driver IC (MAX3353) is used. With this chip you can monitor the ID signal in two ways:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;1-&lt;/STRONG&gt; Using the ID_OUT pin of external driver IC.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;2-&lt;/STRONG&gt; Reading the ID status via the I2C communication with the driver IC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Some reference boards as &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=TWR-K20D50M&amp;amp;tid=m32TWR"&gt;&lt;STRONG&gt;TWR-K20D50M&lt;/STRONG&gt;&lt;/A&gt; already have the USB_ID pin connected to a GPIO so that it can be monitored by the application.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For more details on this check the next thread:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/311766"&gt;K60 USB FS/LS OTG Controller: Few questions&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps with your doubt.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Oct 2014 02:15:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MD20DX128VFM5-USB-ID-Pin/m-p/371096#M19282</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2014-10-07T02:15:24Z</dc:date>
    </item>
  </channel>
</rss>