<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: KL15 UART Stop Bit Issue in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL15-UART-Stop-Bit-Issue/m-p/370907#M19253</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yonggon,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There without UART stop bit errata info of KL15 product.&lt;/P&gt;&lt;P&gt;I would recommend customer to refer Kinetis L series product UART module validation code for a reference.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;best regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 26 Dec 2014 08:52:12 GMT</pubDate>
    <dc:creator>Hui_Ma</dc:creator>
    <dc:date>2014-12-26T08:52:12Z</dc:date>
    <item>
      <title>KL15 UART Stop Bit Issue</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL15-UART-Stop-Bit-Issue/m-p/370906#M19252</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to read UART signal with 38400 Baud, 9 bit data, 1 stop bit and noticed that characters are missed every few characters. After setting a bit output to generate a short pulse&amp;nbsp; for RX interrupt, I did confirm that the interrupt signal is not generated for every few characters, especially those following 0x00 character. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can I resolve this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yonggon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Dec 2014 19:45:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL15-UART-Stop-Bit-Issue/m-p/370906#M19252</guid>
      <dc:creator>ylee</dc:creator>
      <dc:date>2014-12-22T19:45:38Z</dc:date>
    </item>
    <item>
      <title>Re: KL15 UART Stop Bit Issue</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL15-UART-Stop-Bit-Issue/m-p/370907#M19253</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yonggon,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There without UART stop bit errata info of KL15 product.&lt;/P&gt;&lt;P&gt;I would recommend customer to refer Kinetis L series product UART module validation code for a reference.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;best regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Dec 2014 08:52:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL15-UART-Stop-Bit-Issue/m-p/370907#M19253</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2014-12-26T08:52:12Z</dc:date>
    </item>
  </channel>
</rss>