<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックmsCAN BUS</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/msCAN-BUS/m-p/369820#M19127</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to listen for special devices via the can bus.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To begin learning i am use with two KINETIS FRDM boards those communicates one with other.and run demo project .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My main issue how i can set and define the mask identification for listen another device with Extended ID &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to receive some advice's for start .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 Aug 2014 08:05:17 GMT</pubDate>
    <dc:creator>boriszviagin</dc:creator>
    <dc:date>2014-08-20T08:05:17Z</dc:date>
    <item>
      <title>msCAN BUS</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/msCAN-BUS/m-p/369820#M19127</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to listen for special devices via the can bus.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;To begin learning i am use with two KINETIS FRDM boards those communicates one with other.and run demo project .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My main issue how i can set and define the mask identification for listen another device with Extended ID &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to receive some advice's for start .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Aug 2014 08:05:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/msCAN-BUS/m-p/369820#M19127</guid>
      <dc:creator>boriszviagin</dc:creator>
      <dc:date>2014-08-20T08:05:17Z</dc:date>
    </item>
    <item>
      <title>Re: msCAN BUS</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/msCAN-BUS/m-p/369821#M19128</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check to use MSCAN_CANIDMRn register (MSCAN Identifier Mask Register n of First Bank).&lt;/P&gt;&lt;P&gt;Such as below picture shows how to set related register to filter extended ID ():&lt;/P&gt;&lt;P&gt;To receive standard identifiers in 32-bit filter mode, it is required to program the last three bits (AM[2:0]) in the mask registers CANIDMR3 to "don't care."&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/40422i597FFF0A37DFE39F/image-size/large?v=v2&amp;amp;px=999" title="CAN.png" alt="CAN.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;For you want to receive all Extended ID CAN frame, it need to set CANIDMR[0~3] registers all to 0xFF.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;BR /&gt;best regards &lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Aug 2014 08:50:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/msCAN-BUS/m-p/369821#M19128</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2014-08-22T08:50:31Z</dc:date>
    </item>
  </channel>
</rss>