<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: K64F I2C ACK</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64F-I2C-ACK/m-p/368518#M19038</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Maya,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When you set the slave address to 0x00, which in fact send a START BYTE.&lt;/P&gt;&lt;P&gt;Please check below picture about I2C first byte definition:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="START.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/49503i8E92DDDA00392D46/image-size/large?v=v2&amp;amp;px=999" role="button" title="START.png" alt="START.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;In this case, there with below start procedure:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="START1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/49504i8C09705237892D6C/image-size/large?v=v2&amp;amp;px=999" role="button" title="START1.png" alt="START1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;From I2C bus specification, An acknowledge-related clock pulse is generated after the START byte. &lt;/P&gt;&lt;P&gt;This is present only to conform with the byte handling format used on the bus. No device is allowed to acknowledge the START byte.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So you observe signal is normal.&lt;/P&gt;&lt;P&gt;More detailed info, please check with I2C bus specification page 17.&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;best regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 23 Jan 2015 09:17:24 GMT</pubDate>
    <dc:creator>Hui_Ma</dc:creator>
    <dc:date>2015-01-23T09:17:24Z</dc:date>
    <item>
      <title>K64F I2C ACK</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64F-I2C-ACK/m-p/368517#M19037</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Experts,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I downloaded the K64 sample code for tower board (Kinetis_K64_SC_INIT) from the web site and just changed the slave address to 0x00. And I just pulled up the I2C1 line, PTC10 and PTC11. There is no I2C device. However I saw some "Ack"s (Please refer the attached picture)... Is it normal? or any register setting would be wrong?? I added ODE=1 code into the sample code but there is no change..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using a FRDM-K64F(revB, sch revD1), not tower board. But I thought the sample code would work on FRDM-K64F as well...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Maya&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Jan 2015 09:56:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64F-I2C-ACK/m-p/368517#M19037</guid>
      <dc:creator>mayawatanabe</dc:creator>
      <dc:date>2015-01-22T09:56:01Z</dc:date>
    </item>
    <item>
      <title>Re: K64F I2C ACK</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64F-I2C-ACK/m-p/368518#M19038</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Maya,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When you set the slave address to 0x00, which in fact send a START BYTE.&lt;/P&gt;&lt;P&gt;Please check below picture about I2C first byte definition:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="START.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/49503i8E92DDDA00392D46/image-size/large?v=v2&amp;amp;px=999" role="button" title="START.png" alt="START.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;In this case, there with below start procedure:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="START1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/49504i8C09705237892D6C/image-size/large?v=v2&amp;amp;px=999" role="button" title="START1.png" alt="START1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;From I2C bus specification, An acknowledge-related clock pulse is generated after the START byte. &lt;/P&gt;&lt;P&gt;This is present only to conform with the byte handling format used on the bus. No device is allowed to acknowledge the START byte.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So you observe signal is normal.&lt;/P&gt;&lt;P&gt;More detailed info, please check with I2C bus specification page 17.&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;best regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Jan 2015 09:17:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64F-I2C-ACK/m-p/368518#M19038</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2015-01-23T09:17:24Z</dc:date>
    </item>
  </channel>
</rss>