<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: What IDE do you recommend with TWR-K60D100M</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-IDE-do-you-recommend-with-TWR-K60D100M/m-p/366863#M18907</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pablo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can use CodeWarrior 10.6. I have developsome applications using K60 and it worked well for me. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind Regards&lt;/P&gt;&lt;P&gt;Amit&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 Mar 2015 03:49:14 GMT</pubDate>
    <dc:creator>Amit_Kumar1</dc:creator>
    <dc:date>2015-03-12T03:49:14Z</dc:date>
    <item>
      <title>What IDE do you recommend with TWR-K60D100M</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-IDE-do-you-recommend-with-TWR-K60D100M/m-p/366860#M18904</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am very new to developing with freescale (have done some NXP before)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you point me to the best IDE and best starting place for developing with TWR-K60D100M?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems that this is not supported in KDS - I just want to start working with the best IDE - MKD requires you to pay to build large applications which I will be doing soon.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also have a TWR-IND-IO board and I would like to start working with CAN on this. (perhaps using MQX as OS as well)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any pointers will be appreciated&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your help&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 08 Mar 2015 00:15:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-IDE-do-you-recommend-with-TWR-K60D100M/m-p/366860#M18904</guid>
      <dc:creator>pablomolina</dc:creator>
      <dc:date>2015-03-08T00:15:17Z</dc:date>
    </item>
    <item>
      <title>Re: What IDE do you recommend with TWR-K60D100M</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-IDE-do-you-recommend-with-TWR-K60D100M/m-p/366861#M18905</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pablo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;See &lt;A href="http://www.utasker.com/kinetis.html" title="http://www.utasker.com/kinetis.html"&gt;µTasker Kinetis support&lt;/A&gt; for a list of IDEs.&lt;/P&gt;&lt;P&gt;You can use CodeWarrior 10.x for up to 128k code (enough for most work)&lt;/P&gt;&lt;P&gt;Another completely free one is CooCox but you will have to check on the laster Kinetis debugger support in it.&lt;/P&gt;&lt;P&gt;You can also work with VisualStudio Express and GCC - without debugger it is free. There is a GDB debugger for it but it costs a little, and requires you to have the full VS version too.&lt;/P&gt;&lt;P&gt;It is still possible to work with KDS - it may have a few debugger restrictions since it is aimed at newer devices - but it can still work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you have a small budge available (that is rather than $0 being the top-end) check out Rowley Crossworks since it is well prices and powerful.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kinetis: &lt;A href="http://www.utasker.com/kinetis.html" title="http://www.utasker.com/kinetis.html"&gt;µTasker Kinetis support&lt;/A&gt;&lt;/P&gt;&lt;P&gt;K60: &lt;A href="http://www.utasker.com/kinetis/TWR-K60N512.html" title="http://www.utasker.com/kinetis/TWR-K60N512.html"&gt;µTasker Kinetis TWR-K60N512 support&lt;/A&gt; / &lt;A href="http://www.utasker.com/kinetis/TWR-K60D100M.html" title="http://www.utasker.com/kinetis/TWR-K60D100M.html"&gt;µTasker Kinetis TWR-K60D100M support&lt;/A&gt; / &lt;A href="http://www.utasker.com/kinetis/TWR-K60F120M.html" title="http://www.utasker.com/kinetis/TWR-K60F120M.html"&gt;µTasker Kinetis TWR-K60F120M support&lt;/A&gt;&lt;/P&gt;&lt;P&gt;CAN: &lt;A href="http://www.utasker.com/docs/uTasker/uTaskerCAN.PDF" title="http://www.utasker.com/docs/uTasker/uTaskerCAN.PDF"&gt;http://www.utasker.com/docs/uTasker/uTaskerCAN.PDF&lt;/A&gt; / &lt;A href="https://www.youtube.com/watch?v=Ha8cv_XEvco" title="https://www.youtube.com/watch?v=Ha8cv_XEvco"&gt;FlexCAN.wmv - YouTube&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;For the complete "out-of-the-box" Kinetis experience and faster time to market &lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 08 Mar 2015 02:08:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-IDE-do-you-recommend-with-TWR-K60D100M/m-p/366861#M18905</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2015-03-08T02:08:02Z</dc:date>
    </item>
    <item>
      <title>Re: What IDE do you recommend with TWR-K60D100M</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-IDE-do-you-recommend-with-TWR-K60D100M/m-p/366862#M18906</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your answer Mark.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I actually find out that the TWR-k60D100M is supported in the new KSDK 1.1 version on KDS&lt;/P&gt;&lt;P&gt;This are the steps I followed:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) Install KDS&lt;/P&gt;&lt;P&gt;2) Download and install KSDK 1.1&lt;/P&gt;&lt;P&gt;3) Follow the guide on the KSDK manuals&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am now having other problems, but I successfully build and programmed the device from KDS&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 08 Mar 2015 23:13:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-IDE-do-you-recommend-with-TWR-K60D100M/m-p/366862#M18906</guid>
      <dc:creator>pablomolina</dc:creator>
      <dc:date>2015-03-08T23:13:40Z</dc:date>
    </item>
    <item>
      <title>Re: What IDE do you recommend with TWR-K60D100M</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-IDE-do-you-recommend-with-TWR-K60D100M/m-p/366863#M18907</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pablo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can use CodeWarrior 10.6. I have developsome applications using K60 and it worked well for me. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind Regards&lt;/P&gt;&lt;P&gt;Amit&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Mar 2015 03:49:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/What-IDE-do-you-recommend-with-TWR-K60D100M/m-p/366863#M18907</guid>
      <dc:creator>Amit_Kumar1</dc:creator>
      <dc:date>2015-03-12T03:49:14Z</dc:date>
    </item>
  </channel>
</rss>