<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Using CMSIS -&amp;gt; No such file ARMCM4.h? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-CMSIS-gt-No-such-file-ARMCM4-h/m-p/366346#M18880</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Playing around with the FRDM_K22F and got the KSDK demo apps to compile, load and debug.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now moving on to the next step of using the CMSIS DSP functions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Not sure how to reference these in my demo project. Can someone point me to the steps required to successfully use the CMSIS libraries in my project in KDS?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried to include the CMSIS directory from the KSDK directory in the project but during the build it complains that ARMCM4.h is missing. Looking through the KSDK tree there does not seem to be an any file with that name?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any tutorial to get CMSIS DSP up and running?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 19 Aug 2014 05:00:14 GMT</pubDate>
    <dc:creator>marcohess</dc:creator>
    <dc:date>2014-08-19T05:00:14Z</dc:date>
    <item>
      <title>Using CMSIS -&gt; No such file ARMCM4.h?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-CMSIS-gt-No-such-file-ARMCM4-h/m-p/366346#M18880</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Playing around with the FRDM_K22F and got the KSDK demo apps to compile, load and debug.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now moving on to the next step of using the CMSIS DSP functions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Not sure how to reference these in my demo project. Can someone point me to the steps required to successfully use the CMSIS libraries in my project in KDS?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried to include the CMSIS directory from the KSDK directory in the project but during the build it complains that ARMCM4.h is missing. Looking through the KSDK tree there does not seem to be an any file with that name?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any tutorial to get CMSIS DSP up and running?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Aug 2014 05:00:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-CMSIS-gt-No-such-file-ARMCM4-h/m-p/366346#M18880</guid>
      <dc:creator>marcohess</dc:creator>
      <dc:date>2014-08-19T05:00:14Z</dc:date>
    </item>
    <item>
      <title>Re: Using CMSIS -&gt; No such file ARMCM4.h?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-CMSIS-gt-No-such-file-ARMCM4-h/m-p/366347#M18881</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Marco Hess&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This Link Might me helpful to you. &lt;A href="https://community.nxp.com/thread/324740"&gt;Interfacing CMSIS Library in Codewarrior?&lt;/A&gt;&amp;nbsp;&amp;nbsp; It Is tested in Cw 10.5 and Cw 10.6 with FRDM board and I have tested CMSIS 3.2 Lib, CMSIS 4.0.0 Lib,&amp;nbsp; and CMSIS 4.0.1 Lib. CMSIS 3.2 may work easily but the higher version&amp;nbsp; had issues of memory overflowing so keep that in mind.&amp;nbsp; I think uneed to first build the lib. and then link the build lib. in your project. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Amit Kumar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Aug 2014 04:43:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-CMSIS-gt-No-such-file-ARMCM4-h/m-p/366347#M18881</guid>
      <dc:creator>Amit_Kumar1</dc:creator>
      <dc:date>2014-08-20T04:43:34Z</dc:date>
    </item>
    <item>
      <title>Re: Using CMSIS -&gt; No such file ARMCM4.h?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-CMSIS-gt-No-such-file-ARMCM4-h/m-p/366348#M18882</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I found the ARMCM4.h file in the CMSIS library package downloaded from ARM in:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Device/ARM/ARMCM4/Include&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And then managed to reference that include path in my project and then add the reference to the ARM math library as included in the KSDK for the linger and get my app to compile and run.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This seems to work when I cut and paste some of the ARM CMSIS example code in my app.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Nevertheless I find it strange that the KSDK contains the ARM CMSIS-DSP source files but not the required ARM header files to compile these?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Seems like a bug in the KSDK to me.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Aug 2014 07:53:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-CMSIS-gt-No-such-file-ARMCM4-h/m-p/366348#M18882</guid>
      <dc:creator>marcohess</dc:creator>
      <dc:date>2014-08-20T07:53:36Z</dc:date>
    </item>
    <item>
      <title>Re: Using CMSIS -&gt; No such file ARMCM4.h?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-CMSIS-gt-No-such-file-ARMCM4-h/m-p/366349#M18883</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Marco,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The sai_demo can provide a good template for how to use the CMSIS-DSP libraries with KDS. I suggest making sure the Properties-&amp;gt;C/C++ Build-&amp;gt;Settings in your project are similar to the sai_demo. For instance, the compiler tries to locate&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt; ARMCM4.h&lt;/SPAN&gt; unless you define ARM_MATH_CM4 (or another Cortex-M core) in the C compiler preprocessor. &lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;ARMCM4.h&lt;/SPAN&gt; is the header file that arm_math.h tries to include by default if no Cortex-M core has been defined.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ARMCM4.h is a generic Cortex-M4 device header file, it is not included in KSDK because we use the Kinetis device specific header files.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Martyn&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Aug 2014 16:47:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Using-CMSIS-gt-No-such-file-ARMCM4-h/m-p/366349#M18883</guid>
      <dc:creator>martynhunt</dc:creator>
      <dc:date>2014-08-20T16:47:03Z</dc:date>
    </item>
  </channel>
</rss>