<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックWhich CAN interface does FRDM-KE06Z supports?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-CAN-interface-does-FRDM-KE06Z-supports/m-p/365560#M18815</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I wanted to know if the CAN present in FRDM-KE06Z supports &lt;/P&gt;&lt;P&gt;1) 29 bit ID frame&lt;/P&gt;&lt;P&gt;2) CAN-FD (CAN with Flexible Data rate)&lt;/P&gt;&lt;P&gt;3) Is it possible for this board to communicate with K60 series using CAN?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind Regards&lt;/P&gt;&lt;P&gt;Amit&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Feb 2015 08:53:22 GMT</pubDate>
    <dc:creator>Amit_Kumar1</dc:creator>
    <dc:date>2015-02-11T08:53:22Z</dc:date>
    <item>
      <title>Which CAN interface does FRDM-KE06Z supports?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-CAN-interface-does-FRDM-KE06Z-supports/m-p/365560#M18815</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I wanted to know if the CAN present in FRDM-KE06Z supports &lt;/P&gt;&lt;P&gt;1) 29 bit ID frame&lt;/P&gt;&lt;P&gt;2) CAN-FD (CAN with Flexible Data rate)&lt;/P&gt;&lt;P&gt;3) Is it possible for this board to communicate with K60 series using CAN?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind Regards&lt;/P&gt;&lt;P&gt;Amit&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Feb 2015 08:53:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-CAN-interface-does-FRDM-KE06Z-supports/m-p/365560#M18815</guid>
      <dc:creator>Amit_Kumar1</dc:creator>
      <dc:date>2015-02-11T08:53:22Z</dc:date>
    </item>
    <item>
      <title>Re: Which CAN interface does FRDM-KE06Z supports?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-CAN-interface-does-FRDM-KE06Z-supports/m-p/365561#M18816</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your interest in Freescale Kinetis product, I would like to provide service for you!&lt;/P&gt;&lt;P&gt;1: Yes, KE06 supports 29bit ID frame by setting the ID extended bit in the according register.&lt;/P&gt;&lt;P&gt;&amp;nbsp; About details, please check the KE06 reference manual.&lt;/P&gt;&lt;P&gt;2: KE06 have MSCAN module, it is implementing the CAN 2.0A/B protocal, it isn't the CAN-FD.&lt;/P&gt;&lt;P&gt;3. If you want to using CAN communicate the KE06 with K60, you should use the CAN bus Transceivers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;If you still have question, please let me know!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jingjing&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Feb 2015 02:18:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-CAN-interface-does-FRDM-KE06Z-supports/m-p/365561#M18816</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2015-02-12T02:18:17Z</dc:date>
    </item>
    <item>
      <title>Re: Which CAN interface does FRDM-KE06Z supports?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-CAN-interface-does-FRDM-KE06Z-supports/m-p/365562#M18817</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jingjing&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the quick response.&lt;/P&gt;&lt;P&gt;1. In FRDM_KE06Z board, The CAN trans-receiver is present i.e &lt;STRONG&gt;SN65HVD230D, &lt;/STRONG&gt;I think that should do the job. What do you suggest?&lt;/P&gt;&lt;P&gt;2. What is the difference in MSCAN and CAN present in K60 uc? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Amit&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Feb 2015 04:31:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-CAN-interface-does-FRDM-KE06Z-supports/m-p/365562#M18817</guid>
      <dc:creator>Amit_Kumar1</dc:creator>
      <dc:date>2015-02-12T04:31:55Z</dc:date>
    </item>
    <item>
      <title>Re: Which CAN interface does FRDM-KE06Z supports?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-CAN-interface-does-FRDM-KE06Z-supports/m-p/365563#M18818</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Amit Kumar,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1. Yes, you can use &lt;STRONG&gt;SN65HVD230D&lt;/STRONG&gt; as trans-receiver.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 2. FlexCan is more flexible than Mscan, the FlexCAN module contains much more sophisticated state machine than the MSCAN module.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; FlexCAN can automatically respond to a remote frame.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; About more details, please compare the features in the KE06 and K60 reference manual.&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jingjing&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Feb 2015 06:15:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-CAN-interface-does-FRDM-KE06Z-supports/m-p/365563#M18818</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2015-02-12T06:15:17Z</dc:date>
    </item>
    <item>
      <title>Re: Which CAN interface does FRDM-KE06Z supports?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-CAN-interface-does-FRDM-KE06Z-supports/m-p/365564#M18819</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks For the update.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Feb 2015 06:20:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Which-CAN-interface-does-FRDM-KE06Z-supports/m-p/365564#M18819</guid>
      <dc:creator>Amit_Kumar1</dc:creator>
      <dc:date>2015-02-12T06:20:15Z</dc:date>
    </item>
  </channel>
</rss>