<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Windows 8.1 and AN4379 boot-loader file write</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Windows-8-1-and-AN4379-boot-loader-file-write/m-p/365431#M18790</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Alex&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;See:&lt;/P&gt;&lt;P&gt;- &lt;A href="https://community.nxp.com/message/419530"&gt;Re: AN4379 cannot bootload a program  &amp;amp;gt; 25 kB&lt;/A&gt;&lt;/P&gt;&lt;P&gt;- &lt;A href="https://community.nxp.com/message/388866"&gt;Re: AN3927 USB MSD Bootloader - does it work on Windows 8 or 8.1?&lt;/A&gt;&lt;/P&gt;&lt;P&gt;See whether disabling teh following helps: &lt;A href="http://answers.microsoft.com/en-us/windows/forum/windows8_1-hardware/how-do-i-prevent-system-volume-information-files/815b0046-d631-4419-a43e-44083a3733f5?page=2" title="http://answers.microsoft.com/en-us/windows/forum/windows8_1-hardware/how-do-i-prevent-system-volume-information-files/815b0046-d631-4419-a43e-44083a3733f5?page=2"&gt;http://answers.microsoft.com/en-us/windows/forum/windows8_1-hardware/how-do-i-prevent-system-volume-information-files/815b0046-d631-4419-a43e-44083a3733f5?page=2&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note that the following version also shows file name and date, plus allow password protected copying back of the software (compatible with Windows 8.1): &lt;A href="https://community.nxp.com/message/377071"&gt;Re: Kinetis Boot Loader for SREC UART, SD Card and USB-MSD loading&lt;/A&gt; Shown in the video: &lt;A href="https://www.youtube.com/watch?v=XVlCisUmJMI&amp;amp;feature=youtu.be" title="https://www.youtube.com/watch?v=XVlCisUmJMI&amp;amp;feature=youtu.be"&gt;Kinetis K60 Tower Kit - Flexible Boot Loader - YouTube&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Now it also allow mixing with KBOOT HID.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 24 Nov 2014 19:19:32 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2014-11-24T19:19:32Z</dc:date>
    <item>
      <title>Windows 8.1 and AN4379 boot-loader file write</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Windows-8-1-and-AN4379-boot-loader-file-write/m-p/365430#M18789</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have adapted AN4379 boot-loader for our product.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Upgrading the product firmware by copying an S19 image file to the product when enumerated as a hard drive has worked perfectly on Windows 7 and Windows XP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Evaluating the same process on a Windows 8.1 machine results in a file copy failure near the end of the S19 file (seen on USB analyzer).&amp;nbsp; There is still a significant number of S19 entries to send.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The process stops, and a reset is sent by the PC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Notes.&lt;/P&gt;&lt;P&gt;1.&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; The boot-loader firmware has been adapted to remember root directory writes, and show up-to-date file names on the hard drive window.&lt;/P&gt;&lt;P&gt;2.&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; The Bulk packet in/out sizes have been changed from 32 bytes to 64 bytes.&amp;nbsp; This has not affected the described behavior.&lt;/P&gt;&lt;P&gt;3.&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; The Windows 8.1 machine has been fully upgraded.&amp;nbsp; Some Googling showed that system file USBSTOR.SYS has been changed recently due to complaints about external USB drives being powered down during use.&lt;/P&gt;&lt;P&gt;4.&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Trying to write a small S19 file (approx. 62kB vs. 800kB) still fails near the end of the file.&lt;/P&gt;&lt;P&gt;5.&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Kinetis K20 part.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any suggestions would be most welcome!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Nov 2014 16:23:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Windows-8-1-and-AN4379-boot-loader-file-write/m-p/365430#M18789</guid>
      <dc:creator>leccy</dc:creator>
      <dc:date>2014-11-24T16:23:22Z</dc:date>
    </item>
    <item>
      <title>Re: Windows 8.1 and AN4379 boot-loader file write</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Windows-8-1-and-AN4379-boot-loader-file-write/m-p/365431#M18790</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Alex&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;See:&lt;/P&gt;&lt;P&gt;- &lt;A href="https://community.nxp.com/message/419530"&gt;Re: AN4379 cannot bootload a program  &amp;amp;gt; 25 kB&lt;/A&gt;&lt;/P&gt;&lt;P&gt;- &lt;A href="https://community.nxp.com/message/388866"&gt;Re: AN3927 USB MSD Bootloader - does it work on Windows 8 or 8.1?&lt;/A&gt;&lt;/P&gt;&lt;P&gt;See whether disabling teh following helps: &lt;A href="http://answers.microsoft.com/en-us/windows/forum/windows8_1-hardware/how-do-i-prevent-system-volume-information-files/815b0046-d631-4419-a43e-44083a3733f5?page=2" title="http://answers.microsoft.com/en-us/windows/forum/windows8_1-hardware/how-do-i-prevent-system-volume-information-files/815b0046-d631-4419-a43e-44083a3733f5?page=2"&gt;http://answers.microsoft.com/en-us/windows/forum/windows8_1-hardware/how-do-i-prevent-system-volume-information-files/815b0046-d631-4419-a43e-44083a3733f5?page=2&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note that the following version also shows file name and date, plus allow password protected copying back of the software (compatible with Windows 8.1): &lt;A href="https://community.nxp.com/message/377071"&gt;Re: Kinetis Boot Loader for SREC UART, SD Card and USB-MSD loading&lt;/A&gt; Shown in the video: &lt;A href="https://www.youtube.com/watch?v=XVlCisUmJMI&amp;amp;feature=youtu.be" title="https://www.youtube.com/watch?v=XVlCisUmJMI&amp;amp;feature=youtu.be"&gt;Kinetis K60 Tower Kit - Flexible Boot Loader - YouTube&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Now it also allow mixing with KBOOT HID.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Nov 2014 19:19:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Windows-8-1-and-AN4379-boot-loader-file-write/m-p/365431#M18790</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2014-11-24T19:19:32Z</dc:date>
    </item>
  </channel>
</rss>