<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックCLOCK_SYS_GetBusClockFreq() returns 0 in KSDK 1.1</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CLOCK-SYS-GetBusClockFreq-returns-0-in-KSDK-1-1/m-p/365313#M18785</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I ported a project from KSDK 1.0 to 1.1 (in KDS 2.0) and am running into some trouble during the PDB initialisation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Previously using KSDK 1.0, CLOCK_SYS_GetBusClockFreq() returned the correct 60MHz and I can calculate the correct PDB MOD value.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now with KSDK 1.1 it returns 0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I traced through the &lt;SPAN style="font-size: 13.3333330154419px;"&gt;CLOCK_SYS_GetBusClockFreq() call but it goes through so many levels of lower level functions, I can't make sense of it anymore.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What's wrong?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Feb 2015 05:43:13 GMT</pubDate>
    <dc:creator>marcohess</dc:creator>
    <dc:date>2015-02-11T05:43:13Z</dc:date>
    <item>
      <title>CLOCK_SYS_GetBusClockFreq() returns 0 in KSDK 1.1</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CLOCK-SYS-GetBusClockFreq-returns-0-in-KSDK-1-1/m-p/365313#M18785</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I ported a project from KSDK 1.0 to 1.1 (in KDS 2.0) and am running into some trouble during the PDB initialisation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Previously using KSDK 1.0, CLOCK_SYS_GetBusClockFreq() returned the correct 60MHz and I can calculate the correct PDB MOD value.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now with KSDK 1.1 it returns 0.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I traced through the &lt;SPAN style="font-size: 13.3333330154419px;"&gt;CLOCK_SYS_GetBusClockFreq() call but it goes through so many levels of lower level functions, I can't make sense of it anymore.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What's wrong?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Feb 2015 05:43:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/CLOCK-SYS-GetBusClockFreq-returns-0-in-KSDK-1-1/m-p/365313#M18785</guid>
      <dc:creator>marcohess</dc:creator>
      <dc:date>2015-02-11T05:43:13Z</dc:date>
    </item>
    <item>
      <title>Re: CLOCK_SYS_GetBusClockFreq() returns 0 in KSDK 1.1</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CLOCK-SYS-GetBusClockFreq-returns-0-in-KSDK-1-1/m-p/365314#M18786</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Marco,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You'd better don't&amp;nbsp; port the KSDK1.0 project to KSDK1.1, they are not incompatible.&lt;/P&gt;&lt;P&gt;Sorry for&amp;nbsp; the inconvenient for you !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alice&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Feb 2015 06:40:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/CLOCK-SYS-GetBusClockFreq-returns-0-in-KSDK-1-1/m-p/365314#M18786</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2015-02-11T06:40:32Z</dc:date>
    </item>
    <item>
      <title>Re: CLOCK_SYS_GetBusClockFreq() returns 0 in KSDK 1.1</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CLOCK-SYS-GetBusClockFreq-returns-0-in-KSDK-1-1/m-p/365315#M18787</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In the mean time I found I needed the following in my hardware_init():&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Setup board clock source. */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; g_xtal0ClkFreq = 8000000U;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; g_xtalRtcClkFreq = 32768U;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The bus clock now properly returns the 60MHz value I was expecting.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But I am stilling having trouble with the PDB when I enable the DMA trigger of the PDB.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Feb 2015 07:28:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/CLOCK-SYS-GetBusClockFreq-returns-0-in-KSDK-1-1/m-p/365315#M18787</guid>
      <dc:creator>marcohess</dc:creator>
      <dc:date>2015-02-11T07:28:49Z</dc:date>
    </item>
    <item>
      <title>Re: CLOCK_SYS_GetBusClockFreq() returns 0 in KSDK 1.1</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/CLOCK-SYS-GetBusClockFreq-returns-0-in-KSDK-1-1/m-p/365316#M18788</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Marco,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The driver function between SDK1.0 and SDK1.1 are different , so it hared to porting .&lt;/P&gt;&lt;P&gt;So recommend create a new project about SDK 1.1 refer to the previous project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Feb 2015 09:03:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/CLOCK-SYS-GetBusClockFreq-returns-0-in-KSDK-1-1/m-p/365316#M18788</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2015-02-11T09:03:45Z</dc:date>
    </item>
  </channel>
</rss>