<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Need help getting started in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Need-help-getting-started/m-p/365297#M18781</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bob,&lt;/P&gt;&lt;P&gt;You can design the minimum circuit for MKE06Z128VLD4 by referring to the SCH of the FRDM-KE06Z board and you needn't to consider some extra requirements.&lt;/P&gt;&lt;P&gt;I've sharing a thread with you about using the Freedom board as SWD program and please refer to it for details.&lt;/P&gt;&lt;P&gt;David also shared much experience and it's very helpful for accelerating start with Kinetis MCU.&lt;/P&gt;&lt;P&gt;&lt;A href="http://mcuoneclipse.com/2013/04/21/using-the-freedom-board-as-jtag-programmer/" title="http://mcuoneclipse.com/2013/04/21/using-the-freedom-board-as-jtag-programmer/"&gt;http://mcuoneclipse.com/2013/04/21/using-the-freedom-board-as-jtag-programmer/&lt;/A&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 09 Mar 2015 09:02:14 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2015-03-09T09:02:14Z</dc:date>
    <item>
      <title>Need help getting started</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Need-help-getting-started/m-p/365295#M18779</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm looking to switch to the Kinetis chips from PIC32s. My plan is to make my own boards with the MKE06Z128VLD4 and program them with the FRDM-KE06Z. I would use Kinetis Design Studio.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've looked through the data sheet and reference manual (admittedly just the table of contents) and have not found a schematic for the minimum circuit requirements to get the MKE06Z128VLD4 running (power, ground, bypass caps, SWD connections). Is there such a document available?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've also seen mixed claims about the Freedom boards' use as SWD programmer/debuggers. Is the FRDM-KE06Z OpenSDA locked to program only specific Kinetis chips, or can it work with any Kinetis? (Probably too much to hope that it can work with any ARM.)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Bob&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Mar 2015 18:23:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Need-help-getting-started/m-p/365295#M18779</guid>
      <dc:creator>robertalexander</dc:creator>
      <dc:date>2015-03-06T18:23:50Z</dc:date>
    </item>
    <item>
      <title>Re: Need help getting started</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Need-help-getting-started/m-p/365296#M18780</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bob, I'm using the KE06128VLH4.&amp;nbsp; It does not have a lot of requirements for getting it going.&amp;nbsp; Only 2 sets of power pins for the core, 1 set for the analog supply.&amp;nbsp; If you don't need CAN, you don't need a crystal.&amp;nbsp; The internal clock source isn't stable enough for CAN.&amp;nbsp;&amp;nbsp; Bear in mind OpenSDA needs another Kinetis microcontroller providing the debugging interface; you would do well to just put the 10 pin header on your production board and use a separate debugger.&amp;nbsp; The OpenSDA is convenient for the FRDM-KE06 board, though you can also populate the debug connector on it and use a separate debugger.&amp;nbsp; I never had any problem using a P&amp;amp;E Multilink with the FRDM-KE06 board; I think the only thing I had to do was remove R35 to run the KE06 at 5 volts, which leaves the OpenSDA out of the picture.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One thing I found the hard way that I'll pass on; if you're using the SPI, the default SPI0_MISO pin (pin 13 on the 44-pin part) also happens to be the NMI pin after reset, and you would do well to put a pull down resistor on it to avoid any unpleasantness. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The SWD header only needs VDD, VSS, /reset, swd_dio, and swd_clk for debugging.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Edit:&amp;nbsp; I forgot, the only glitch I had with using OpenSDA with the FRDM-KE06 involved updating the OpenSDA.&amp;nbsp; Seems to me the default firmware that it comes with only provides the mass storage interface for loading firmware into the target processor; I had to load a different firmware image to get both the mass storage interface and the debug interface.&amp;nbsp; It's not hard to do, but I did have to download something from Freescale to get the update.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Mar 2015 19:20:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Need-help-getting-started/m-p/365296#M18780</guid>
      <dc:creator>davidsherman</dc:creator>
      <dc:date>2015-03-06T19:20:21Z</dc:date>
    </item>
    <item>
      <title>Re: Need help getting started</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Need-help-getting-started/m-p/365297#M18781</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bob,&lt;/P&gt;&lt;P&gt;You can design the minimum circuit for MKE06Z128VLD4 by referring to the SCH of the FRDM-KE06Z board and you needn't to consider some extra requirements.&lt;/P&gt;&lt;P&gt;I've sharing a thread with you about using the Freedom board as SWD program and please refer to it for details.&lt;/P&gt;&lt;P&gt;David also shared much experience and it's very helpful for accelerating start with Kinetis MCU.&lt;/P&gt;&lt;P&gt;&lt;A href="http://mcuoneclipse.com/2013/04/21/using-the-freedom-board-as-jtag-programmer/" title="http://mcuoneclipse.com/2013/04/21/using-the-freedom-board-as-jtag-programmer/"&gt;http://mcuoneclipse.com/2013/04/21/using-the-freedom-board-as-jtag-programmer/&lt;/A&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Mar 2015 09:02:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Need-help-getting-started/m-p/365297#M18781</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2015-03-09T09:02:14Z</dc:date>
    </item>
  </channel>
</rss>