<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: FRDM K64F SPI clock pin problem</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64F-SPI-clock-pin-problem/m-p/365023#M18758</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If the FRDM-K64F has the same digital GND with LCD 5110 board? That could be a root cause.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;BR /&gt;best regards &lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 22 Aug 2014 02:28:17 GMT</pubDate>
    <dc:creator>Hui_Ma</dc:creator>
    <dc:date>2014-08-22T02:28:17Z</dc:date>
    <item>
      <title>FRDM K64F SPI clock pin problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64F-SPI-clock-pin-problem/m-p/365022#M18757</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;I have trouble with serial communication between&amp;nbsp; FRDM K64F and LCD 5110.&lt;/P&gt;&lt;P&gt;When FRDM SPI clock pin (PTD1) is connected to LCD's clock input simply via wire then clock signal&amp;nbsp; stay always low. But if you touch this clock chain in any point by some conductive object (e. g. scope probe or screwdriver) or add to pin some pull-down resistor and reset the board then SPI clock will be generated and LCD work fine.&lt;/P&gt;&lt;P&gt;other spi lines work without problems.&lt;/P&gt;&lt;P&gt;I also checked this LCD with another board&amp;nbsp; and with same wiring everything works fine without any bugs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone explain this behavior?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Aug 2014 16:44:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64F-SPI-clock-pin-problem/m-p/365022#M18757</guid>
      <dc:creator>vubdub</dc:creator>
      <dc:date>2014-08-18T16:44:18Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM K64F SPI clock pin problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64F-SPI-clock-pin-problem/m-p/365023#M18758</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If the FRDM-K64F has the same digital GND with LCD 5110 board? That could be a root cause.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;BR /&gt;best regards &lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Aug 2014 02:28:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64F-SPI-clock-pin-problem/m-p/365023#M18758</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2014-08-22T02:28:17Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM K64F SPI clock pin problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64F-SPI-clock-pin-problem/m-p/365024#M18759</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;here is my wiring&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/43489i4DEFD8F90BA46170/image-size/large?v=v2&amp;amp;px=999" title="Untitled-1.jpg" alt="Untitled-1.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://docs.google.com/file/d/0B8Ca28cJlc3rbnlFTzFXM2NPM1k/edit"&gt;https://docs.google.com/file/d/0B8Ca28cJlc3rbnlFTzFXM2NPM1k/edit&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I also tried to connect display ground to another GND pins on FRDM but it doesn't solve the problem. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Aug 2014 17:42:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64F-SPI-clock-pin-problem/m-p/365024#M18759</guid>
      <dc:creator>vubdub</dc:creator>
      <dc:date>2014-08-22T17:42:40Z</dc:date>
    </item>
  </channel>
</rss>