<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Phantom ILDMAS, UART IDLE line DMA Enable</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Phantom-ILDMAS-UART-IDLE-line-DMA-Enable/m-p/150237#M186</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm afraid that is a documentation error, ILDMAS in UART are not supported in Kinetis microcontrollers.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 07 Feb 2013 14:37:59 GMT</pubDate>
    <dc:creator>apanecatl</dc:creator>
    <dc:date>2013-02-07T14:37:59Z</dc:date>
    <item>
      <title>Phantom ILDMAS, UART IDLE line DMA Enable</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Phantom-ILDMAS-UART-IDLE-line-DMA-Enable/m-p/150236#M185</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt;"&gt;A number of the Kinetis Reference Manuals make reference to 'ILDMAS' in UART register C5.&amp;nbsp; Presumably this would allow DMA generation on an IDLE line condition (instead of an interrupt).&amp;nbsp; But no such bit is shown in the C5 register definition.&amp;nbsp; Was the ILDMAS functionality disabled in Kinetis, or is there a mistake in the manual?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12pt;"&gt;pmt &lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Oct 2012 20:11:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Phantom-ILDMAS-UART-IDLE-line-DMA-Enable/m-p/150236#M185</guid>
      <dc:creator>pmt</dc:creator>
      <dc:date>2012-10-24T20:11:04Z</dc:date>
    </item>
    <item>
      <title>Re: Phantom ILDMAS, UART IDLE line DMA Enable</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Phantom-ILDMAS-UART-IDLE-line-DMA-Enable/m-p/150237#M186</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm afraid that is a documentation error, ILDMAS in UART are not supported in Kinetis microcontrollers.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Feb 2013 14:37:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Phantom-ILDMAS-UART-IDLE-line-DMA-Enable/m-p/150237#M186</guid>
      <dc:creator>apanecatl</dc:creator>
      <dc:date>2013-02-07T14:37:59Z</dc:date>
    </item>
    <item>
      <title>Re: Phantom ILDMAS, UART IDLE line DMA Enable</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Phantom-ILDMAS-UART-IDLE-line-DMA-Enable/m-p/150238#M187</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is someone from Freescale able to share the motivation why the ILDMAS (Idle DMA request) has been removed?&lt;/P&gt;&lt;P&gt;The DMA UART Rx is basically useless without this feature, because the data length which is received from UART is not known in 99% of the use cases...&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/301651"&gt;DISCUSSION:&amp;nbsp; Missing critical RX UART DMA Event Functionality in Freescale Parts&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;FYI: Generating an interrupt on each byte receiption is not an accepted workaround, because this would make the whole DMA use case kind of useless..&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Nov 2015 07:01:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Phantom-ILDMAS-UART-IDLE-line-DMA-Enable/m-p/150238#M187</guid>
      <dc:creator>michaelguntli</dc:creator>
      <dc:date>2015-11-18T07:01:46Z</dc:date>
    </item>
  </channel>
</rss>