<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックK61 USBHS USBn_PWRFAULT signal question</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K61-USBHS-USBn-PWRFAULT-signal-question/m-p/362856#M18540</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using the K61 to support USB High-Speed Host controller.&lt;/P&gt;&lt;P&gt;According to the TWR-K70F120M and TWR-SER2 schematics, the Fault Flag signal of the VBUS switch connected to the VBUS_DT signal of the USB3300 USBHS PHY.&lt;/P&gt;&lt;P&gt;According to the K61 reference manual (K61P256M150SF3RM, Rev 2), the K61USBHS OTG controller will detect over-current condition by below two bit in the USBHS_PORTSC1 register.&lt;/P&gt;&lt;P&gt;- bit 5 OCC&amp;nbsp; Over-Current Change&lt;/P&gt;&lt;P&gt;- bit 4 OCA&amp;nbsp; Over-current active&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But the K61 does not have the USBn_PWRFAULT, and does not connect the Fault Flag signal of the VBUS switch to any pin of the K61.&lt;/P&gt;&lt;P&gt;Here is questions.&lt;/P&gt;&lt;P&gt;1. Can we use the USBHS_PORTSC1 bit 5 OCC and bit 4 OCA to detect over-current condition?&lt;/P&gt;&lt;P&gt;2. To detect over-current condition, should we connect the Fault Flag signal of the VBUS switch to a pin of the K61?&lt;/P&gt;&lt;P&gt;&amp;nbsp; If so, please let us know it pin name.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please reply as soon as possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Takashima&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 Oct 2014 11:55:17 GMT</pubDate>
    <dc:creator>isaotakashima</dc:creator>
    <dc:date>2014-10-02T11:55:17Z</dc:date>
    <item>
      <title>K61 USBHS USBn_PWRFAULT signal question</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K61-USBHS-USBn-PWRFAULT-signal-question/m-p/362856#M18540</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using the K61 to support USB High-Speed Host controller.&lt;/P&gt;&lt;P&gt;According to the TWR-K70F120M and TWR-SER2 schematics, the Fault Flag signal of the VBUS switch connected to the VBUS_DT signal of the USB3300 USBHS PHY.&lt;/P&gt;&lt;P&gt;According to the K61 reference manual (K61P256M150SF3RM, Rev 2), the K61USBHS OTG controller will detect over-current condition by below two bit in the USBHS_PORTSC1 register.&lt;/P&gt;&lt;P&gt;- bit 5 OCC&amp;nbsp; Over-Current Change&lt;/P&gt;&lt;P&gt;- bit 4 OCA&amp;nbsp; Over-current active&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But the K61 does not have the USBn_PWRFAULT, and does not connect the Fault Flag signal of the VBUS switch to any pin of the K61.&lt;/P&gt;&lt;P&gt;Here is questions.&lt;/P&gt;&lt;P&gt;1. Can we use the USBHS_PORTSC1 bit 5 OCC and bit 4 OCA to detect over-current condition?&lt;/P&gt;&lt;P&gt;2. To detect over-current condition, should we connect the Fault Flag signal of the VBUS switch to a pin of the K61?&lt;/P&gt;&lt;P&gt;&amp;nbsp; If so, please let us know it pin name.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please reply as soon as possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Takashima&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Oct 2014 11:55:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K61-USBHS-USBn-PWRFAULT-signal-question/m-p/362856#M18540</guid>
      <dc:creator>isaotakashima</dc:creator>
      <dc:date>2014-10-02T11:55:17Z</dc:date>
    </item>
    <item>
      <title>Re: K61 USBHS USBn_PWRFAULT signal question</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K61-USBHS-USBn-PWRFAULT-signal-question/m-p/362857#M18541</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Takashima,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The VBUS_DT signal of the USB3300 USBHS PHY has nothing with Over-Current condition, it is used to detect the external VBUS availability. so on TWR-SER2, when the VBUS switch detects an external available, it would notify the USB3300 USBHS PHY, which would be reflected in its internal status register.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Jan 2015 08:27:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K61-USBHS-USBn-PWRFAULT-signal-question/m-p/362857#M18541</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2015-01-08T08:27:54Z</dc:date>
    </item>
  </channel>
</rss>