<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 K40 uart PARITY problem</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K40-uart-PARITY-problem/m-p/362029#M18451</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I set up K40 UART3 for 9 data bit and 1 stop bit, parity enable and even parity transmission. However When I transmit modbus data with odd parity or no parity to the K40, it can still receive data perfectly.&lt;/P&gt;&lt;P&gt;the same goes to odd parity or no parity setting.&amp;nbsp; And I verified that UART3_C1 register was showing the correct setting. is there something wrong with this K40 parity ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 Oct 2014 02:46:16 GMT</pubDate>
    <dc:creator>see</dc:creator>
    <dc:date>2014-10-02T02:46:16Z</dc:date>
    <item>
      <title>K40 uart PARITY problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K40-uart-PARITY-problem/m-p/362029#M18451</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I set up K40 UART3 for 9 data bit and 1 stop bit, parity enable and even parity transmission. However When I transmit modbus data with odd parity or no parity to the K40, it can still receive data perfectly.&lt;/P&gt;&lt;P&gt;the same goes to odd parity or no parity setting.&amp;nbsp; And I verified that UART3_C1 register was showing the correct setting. is there something wrong with this K40 parity ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Oct 2014 02:46:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K40-uart-PARITY-problem/m-p/362029#M18451</guid>
      <dc:creator>see</dc:creator>
      <dc:date>2014-10-02T02:46:16Z</dc:date>
    </item>
    <item>
      <title>Re: K40 uart PARITY problem</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K40-uart-PARITY-problem/m-p/362030#M18452</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I checked K40 UART module validation code, which already test UART 9-bit data receive with parity enable. And there is no error reported.&lt;/P&gt;&lt;P&gt;During the UART module validation, it use two UART modules to do 9-bit data transmit and receive.&lt;/P&gt;&lt;P&gt;More detailed info, please check attached UART RX validation code (related validation code located at uart_9bit_rx_test() function).&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Wish it helps.&lt;BR /&gt;best regards &lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Oct 2014 07:30:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K40-uart-PARITY-problem/m-p/362030#M18452</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2014-10-10T07:30:58Z</dc:date>
    </item>
  </channel>
</rss>