<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックSPI Chip Select</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-Chip-Select/m-p/361445#M18367</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using Kinetis MCUs. I wonder if it is possible to connect two SPI slave devices shared the same SS line. One of the SS lines contains a NOT logic gate so I can select the slave device by changing its GPIO value in callback function. Is it possible?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 18 Dec 2014 07:18:57 GMT</pubDate>
    <dc:creator>josephchen</dc:creator>
    <dc:date>2014-12-18T07:18:57Z</dc:date>
    <item>
      <title>SPI Chip Select</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-Chip-Select/m-p/361445#M18367</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using Kinetis MCUs. I wonder if it is possible to connect two SPI slave devices shared the same SS line. One of the SS lines contains a NOT logic gate so I can select the slave device by changing its GPIO value in callback function. Is it possible?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Dec 2014 07:18:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-Chip-Select/m-p/361445#M18367</guid>
      <dc:creator>josephchen</dc:creator>
      <dc:date>2014-12-18T07:18:57Z</dc:date>
    </item>
    <item>
      <title>Re: SPI Chip Select</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-Chip-Select/m-p/361446#M18368</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Joseph，&lt;/P&gt;&lt;P&gt;After learned your statement, I think this scenario can work out.&lt;/P&gt;&lt;P&gt;But I don't consider this method is good enough, I will prefer to share SPI_MISO、SPI_MOSI、SPI_SCLK pin, then use the different GPIO as the SS pin to select the external device.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Jan 2015 02:54:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-Chip-Select/m-p/361446#M18368</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2015-01-06T02:54:29Z</dc:date>
    </item>
  </channel>
</rss>