<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Precise Dimensions of FRDM boards in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Precise-Dimensions-of-FRDM-boards/m-p/361431#M18361</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Kinetis Community:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have been working on making a companion board to the Kinetis FRDM boards that would essentially permit myself or others to make a shield that would connect to the Arduino pins as well as all the pins unique to the various FRDM pin implementations.&amp;nbsp; I can measure my own boards with some degree of precision, but measuring from the the boards is not the best way possible to proceed.&amp;nbsp; These boards, or any manufactured part, are built within certain tolerances.&amp;nbsp; Tolerances are permissible deviations from the intended design, and it is impossible to discern precisely the&amp;nbsp; intended design by measuring the part.&amp;nbsp; Any measurement of the part will always reflect manufacturing variations of the original design, and for various reasons these variations cannot be eliminated..&amp;nbsp; This is important because, if for instance, the object I am measuring was already at the edge of its tolerances, some number of my boards will reflect these errors and will exaggerate these errors due to my own manufacturing errors.&amp;nbsp; My errors will stack on top of the original errors and my result will end up unusable.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The gold standard then is to have a drawing reflecting the original intentions of the designers so that my boards may have the best chance of actually fitting the original FRDM boards reliably.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I started by looking at anything provided by Freescale and the best I was able to learn is that the overall dimensions, the dimensions of the corner radii, and the distance between two of the mounting holes.&amp;nbsp; I also sought out the relationships of the outboard Arduino pins and there too the dimensions are not clear.&amp;nbsp; There are dimensions floating around on various Arduino forums that vary quite a bit.&amp;nbsp; So much so as to be unreliable.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are Freescale PCB files I acquired for the 27556 board, (the production name for the FRDM-KL25Z,) that in some cases are empty files.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So here I am.&amp;nbsp; All I need are some of the original dimensions from Freescale to get going on this, and if I get them, I'd be happy to share my final drawings with the FRDM fan base.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have created a preliminary drawing and I have provided it here in pdf form of the dimensions I've been able to collect and measure on all the FRDM boards. On the attached drawing I have marked with "X" the dimensions I have low confidence IN their correctness.&amp;nbsp; I should also add that the dimensions provided are not the complete set necessary to produce a board that will work with the FRDM boards.&amp;nbsp; It is provided merely to show how few dimensions are actually available out there.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If anyone has a real-deal Freescale drawing of any of the FRDM boards, I sure would appreciate a copy of this file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Tom Sparks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 20 Jan 2015 20:53:01 GMT</pubDate>
    <dc:creator>tomsparks</dc:creator>
    <dc:date>2015-01-20T20:53:01Z</dc:date>
    <item>
      <title>Precise Dimensions of FRDM boards</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Precise-Dimensions-of-FRDM-boards/m-p/361431#M18361</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Kinetis Community:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have been working on making a companion board to the Kinetis FRDM boards that would essentially permit myself or others to make a shield that would connect to the Arduino pins as well as all the pins unique to the various FRDM pin implementations.&amp;nbsp; I can measure my own boards with some degree of precision, but measuring from the the boards is not the best way possible to proceed.&amp;nbsp; These boards, or any manufactured part, are built within certain tolerances.&amp;nbsp; Tolerances are permissible deviations from the intended design, and it is impossible to discern precisely the&amp;nbsp; intended design by measuring the part.&amp;nbsp; Any measurement of the part will always reflect manufacturing variations of the original design, and for various reasons these variations cannot be eliminated..&amp;nbsp; This is important because, if for instance, the object I am measuring was already at the edge of its tolerances, some number of my boards will reflect these errors and will exaggerate these errors due to my own manufacturing errors.&amp;nbsp; My errors will stack on top of the original errors and my result will end up unusable.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The gold standard then is to have a drawing reflecting the original intentions of the designers so that my boards may have the best chance of actually fitting the original FRDM boards reliably.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I started by looking at anything provided by Freescale and the best I was able to learn is that the overall dimensions, the dimensions of the corner radii, and the distance between two of the mounting holes.&amp;nbsp; I also sought out the relationships of the outboard Arduino pins and there too the dimensions are not clear.&amp;nbsp; There are dimensions floating around on various Arduino forums that vary quite a bit.&amp;nbsp; So much so as to be unreliable.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are Freescale PCB files I acquired for the 27556 board, (the production name for the FRDM-KL25Z,) that in some cases are empty files.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So here I am.&amp;nbsp; All I need are some of the original dimensions from Freescale to get going on this, and if I get them, I'd be happy to share my final drawings with the FRDM fan base.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have created a preliminary drawing and I have provided it here in pdf form of the dimensions I've been able to collect and measure on all the FRDM boards. On the attached drawing I have marked with "X" the dimensions I have low confidence IN their correctness.&amp;nbsp; I should also add that the dimensions provided are not the complete set necessary to produce a board that will work with the FRDM boards.&amp;nbsp; It is provided merely to show how few dimensions are actually available out there.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If anyone has a real-deal Freescale drawing of any of the FRDM boards, I sure would appreciate a copy of this file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Tom Sparks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Jan 2015 20:53:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Precise-Dimensions-of-FRDM-boards/m-p/361431#M18361</guid>
      <dc:creator>tomsparks</dc:creator>
      <dc:date>2015-01-20T20:53:01Z</dc:date>
    </item>
    <item>
      <title>Re: Precise Dimensions of FRDM boards</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Precise-Dimensions-of-FRDM-boards/m-p/361432#M18362</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tom,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check below link, The FRDM-TFC is a convenient "shield" that can drive up to two DC motors (5A per channel), two servos and I/O for the Freescale cup line scan camera and Hall effect sensors.&amp;nbsp; This board mates with the &lt;A class="jive-link-external-small" data-content-finding="Community" href="http://www.freescale.com/FRDM-KL25Z"&gt;KL25Z&lt;/A&gt; Freedom board for primary usage with a Freescale Cup car.&lt;/P&gt;&lt;P&gt;There provide component pick place info for your reference.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-93914"&gt;Freescale Cup Shield for the Freedom KL25Z&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;best regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Jan 2015 06:39:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Precise-Dimensions-of-FRDM-boards/m-p/361432#M18362</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2015-01-22T06:39:58Z</dc:date>
    </item>
    <item>
      <title>Re: Precise Dimensions of FRDM boards</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Precise-Dimensions-of-FRDM-boards/m-p/361433#M18363</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hui_Ma:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your help!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tom Sparks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Jan 2015 01:50:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Precise-Dimensions-of-FRDM-boards/m-p/361433#M18363</guid>
      <dc:creator>tomsparks</dc:creator>
      <dc:date>2015-01-30T01:50:56Z</dc:date>
    </item>
  </channel>
</rss>